ProfileBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
ProfileBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.Profile
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateProfileBuilder()
Default values.
Property Value AngleOfRotation.Value 0 AngularTolerance 0.5 BeltAlignment Center DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) EndCutType None EndEndCutBlock.Angle.Value 0 EndEndCutBlock.Offset.Value 0 EndEndCutBlock.SketchBlock.Exp1.Value 0 EndEndCutBlock.SketchBlock.Exp10.Value 0 EndEndCutBlock.SketchBlock.Exp11.Value 0 EndEndCutBlock.SketchBlock.Exp12.Value 0 EndEndCutBlock.SketchBlock.Exp2.Value 0 EndEndCutBlock.SketchBlock.Exp3.Value 0 EndEndCutBlock.SketchBlock.Exp4.Value 0 EndEndCutBlock.SketchBlock.Exp5.Value 0 EndEndCutBlock.SketchBlock.Exp6.Value 0 EndEndCutBlock.SketchBlock.Exp7.Value 0 EndEndCutBlock.SketchBlock.Exp8.Value 0 EndEndCutBlock.SketchBlock.Exp9.Value 0 EndEndCutBlock.SketchBlock.Sketches EndCut1 EndEndCutBlock.TaperType Trim FaceOffsetExpression.Value 0 GuideOffsetExpression.Value 0 KeepFace 0 KeepGuide 0 OrientType FaceNormal PlateHeight.Value 0 PlateWIdth.Value 0 SectionType Profile New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleOfRotation | Returns the angle of rotation |
AngularTolerance | Returns or sets the angular tolerance (degrees). |
AttributeMaterial | Returns or sets the material attribute |
AttributeName | Returns or sets the name attribute value |
BeltAlignment | Returns or sets the belt alignment |
BeltSize | Returns or sets the belt size options |
BeltType | Returns or sets the belt type options |
CurveLengthData | Returns the curve length data |
DistanceTolerance | Returns or sets the distance tolerance (part units). |
EndCutType | Returns or sets the end cut type |
EndEndCutBlock | Returns the end end cut block |
FaceOffsetExpression | Returns the face offset expression |
FaceOffsetVector | Returns or sets the face offset vector |
GuideOffsetExpression | Returns the guide offset expression |
GuideOffsetVector | Returns or sets the guide offset vector |
GuideSection | Returns the select edge |
KeepFace | Returns or sets the toggle which allows re-use of the selected faces |
KeepGuide | Returns or sets the toggle which allows re-use of the selected edges or curves |
OrientType | Returns or sets the orient type |
OrientationVector | Returns or sets the orientation vector |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlateHeight | Returns the plate height |
PlateWIdth | Returns the plate width |
ProfileSize | Returns or sets the profile size options |
ProfileType | Returns or sets the profile type options |
SectionType | Returns or sets the section type |
SelectCsys | Returns the select csys |
SelectFace | Returns the placement faces or datum plane |
StartEndCutBlock | Returns the start end cut block |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type belt or profile |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableAttributeMaterials | Returns the list of available material attributes |
GetAvailableAttributeNames | Returns the list of available name attributes |
GetAvailableBeltSizes | Returns the list of available material attributes |
GetAvailableBeltTypes | Returns the list of available material attributes |
GetAvailableProfileSizes | Returns the list of available material attributes |
GetAvailableProfileTypes | Returns the list of available material attributes |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProfileBuilderAlignment Enumeration | Creation method used to define the placement of the belt this is disabled for profiles |
ProfileBuilderEndCutOption Enumeration | Creation method used to define the end cut type |
ProfileBuilderOrientationOption Enumeration | Creation method used to define the placement of the profile this is disabled for belt creation |
ProfileBuilderSectionOption Enumeration | Creation of profile from the library or a plate |
ProfileBuilderTypeOption Enumeration | Creation type either a belt or a profile |
Property Detail¶
AngleOfRotation¶
-
ProfileBuilder.
AngleOfRotation
¶ Returns the angle of rotation
-------------------------------------
Getter Method
Signature
AngleOfRotation
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: None.
AngularTolerance¶
-
ProfileBuilder.
AngularTolerance
¶ Returns or sets the angular tolerance (degrees).
-------------------------------------
Getter Method
Signature
AngularTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance
Parameters: angularTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
AttributeMaterial¶
-
ProfileBuilder.
AttributeMaterial
¶ Returns or sets the material attribute
-------------------------------------
Getter Method
Signature
AttributeMaterial
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeMaterial
Parameters: material (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
AttributeName¶
-
ProfileBuilder.
AttributeName
¶ Returns or sets the name attribute value
-------------------------------------
Getter Method
Signature
AttributeName
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttributeName
Parameters: name (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
BeltAlignment¶
-
ProfileBuilder.
BeltAlignment
¶ Returns or sets the belt alignment
-------------------------------------
Getter Method
Signature
BeltAlignment
Returns: Return type: NXOpen.Features.ShipDesign.ProfileBuilderAlignment
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeltAlignment
Parameters: beltAlignment ( NXOpen.Features.ShipDesign.ProfileBuilderAlignment
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
BeltSize¶
-
ProfileBuilder.
BeltSize
¶ Returns or sets the belt size options
-------------------------------------
Getter Method
Signature
BeltSize
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeltSize
Parameters: size (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
BeltType¶
-
ProfileBuilder.
BeltType
¶ Returns or sets the belt type options
-------------------------------------
Getter Method
Signature
BeltType
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BeltType
Parameters: type (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
CurveLengthData¶
-
ProfileBuilder.
CurveLengthData
¶ Returns the curve length data
-------------------------------------
Getter Method
Signature
CurveLengthData
Returns: Return type: NXOpen.GeometricUtilities.CurveLengthData
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
ProfileBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance (part units).
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
EndCutType¶
-
ProfileBuilder.
EndCutType
¶ Returns or sets the end cut type
-------------------------------------
Getter Method
Signature
EndCutType
Returns: Return type: NXOpen.Features.ShipDesign.ProfileBuilderEndCutOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutType
Parameters: endCutType ( NXOpen.Features.ShipDesign.ProfileBuilderEndCutOption
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
EndEndCutBlock¶
-
ProfileBuilder.
EndEndCutBlock
¶ Returns the end end cut block
-------------------------------------
Getter Method
Signature
EndEndCutBlock
Returns: Return type: NXOpen.EndCutBlockBuilder
New in version NX7.5.0.
License requirements: None.
FaceOffsetExpression¶
-
ProfileBuilder.
FaceOffsetExpression
¶ Returns the face offset expression
-------------------------------------
Getter Method
Signature
FaceOffsetExpression
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
FaceOffsetVector¶
-
ProfileBuilder.
FaceOffsetVector
¶ Returns or sets the face offset vector
-------------------------------------
Getter Method
Signature
FaceOffsetVector
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceOffsetVector
Parameters: faceOffsetVector (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
GuideOffsetExpression¶
-
ProfileBuilder.
GuideOffsetExpression
¶ Returns the guide offset expression
-------------------------------------
Getter Method
Signature
GuideOffsetExpression
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
GuideOffsetVector¶
-
ProfileBuilder.
GuideOffsetVector
¶ Returns or sets the guide offset vector
-------------------------------------
Getter Method
Signature
GuideOffsetVector
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GuideOffsetVector
Parameters: guideOffsetVector (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
GuideSection¶
-
ProfileBuilder.
GuideSection
¶ Returns the select edge
-------------------------------------
Getter Method
Signature
GuideSection
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
KeepFace¶
-
ProfileBuilder.
KeepFace
¶ Returns or sets the toggle which allows re-use of the selected faces
-------------------------------------
Getter Method
Signature
KeepFace
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepFace
Parameters: keepFace (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
KeepGuide¶
-
ProfileBuilder.
KeepGuide
¶ Returns or sets the toggle which allows re-use of the selected edges or curves
-------------------------------------
Getter Method
Signature
KeepGuide
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepGuide
Parameters: keepGuide (bool) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
OrientType¶
-
ProfileBuilder.
OrientType
¶ Returns or sets the orient type
-------------------------------------
Getter Method
Signature
OrientType
Returns: Return type: NXOpen.Features.ShipDesign.ProfileBuilderOrientationOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientType
Parameters: orientType ( NXOpen.Features.ShipDesign.ProfileBuilderOrientationOption
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
OrientationVector¶
-
ProfileBuilder.
OrientationVector
¶ Returns or sets the orientation vector
-------------------------------------
Getter Method
Signature
OrientationVector
Returns: Return type: NXOpen.Direction
New in version NX7.5.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationVector
Parameters: orientationVector ( NXOpen.Direction
) –New in version NX7.5.4.
License requirements: nx_ship_concept (“Ship Concept”)
PlateHeight¶
-
ProfileBuilder.
PlateHeight
¶ Returns the plate height
-------------------------------------
Getter Method
Signature
PlateHeight
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
PlateWIdth¶
-
ProfileBuilder.
PlateWIdth
¶ Returns the plate width
-------------------------------------
Getter Method
Signature
PlateWIdth
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ProfileSize¶
-
ProfileBuilder.
ProfileSize
¶ Returns or sets the profile size options
-------------------------------------
Getter Method
Signature
ProfileSize
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileSize
Parameters: size (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
ProfileType¶
-
ProfileBuilder.
ProfileType
¶ Returns or sets the profile type options
-------------------------------------
Getter Method
Signature
ProfileType
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProfileType
Parameters: type (int) – New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SectionType¶
-
ProfileBuilder.
SectionType
¶ Returns or sets the section type
-------------------------------------
Getter Method
Signature
SectionType
Returns: Return type: NXOpen.Features.ShipDesign.ProfileBuilderSectionOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SectionType
Parameters: sectionType ( NXOpen.Features.ShipDesign.ProfileBuilderSectionOption
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
SelectCsys¶
-
ProfileBuilder.
SelectCsys
¶ Returns the select csys
-------------------------------------
Getter Method
Signature
SelectCsys
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX7.5.0.
License requirements: None.
SelectFace¶
-
ProfileBuilder.
SelectFace
¶ Returns the placement faces or datum plane
-------------------------------------
Getter Method
Signature
SelectFace
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
StartEndCutBlock¶
-
ProfileBuilder.
StartEndCutBlock
¶ Returns the start end cut block
-------------------------------------
Getter Method
Signature
StartEndCutBlock
Returns: Return type: NXOpen.EndCutBlockBuilder
New in version NX7.5.0.
License requirements: None.
Type¶
-
ProfileBuilder.
Type
¶ Returns or sets the type belt or profile
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.ProfileBuilderTypeOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.ProfileBuilderTypeOption
) –New in version NX7.5.0.
License requirements: nx_ship_concept (“Ship Concept”)
Method Detail¶
GetAvailableAttributeMaterials¶
-
ProfileBuilder.
GetAvailableAttributeMaterials
¶ Returns the list of available material attributes
Signature
GetAvailableAttributeMaterials()
Returns: Array of available attribute materials. These materials are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableAttributeNames¶
-
ProfileBuilder.
GetAvailableAttributeNames
¶ Returns the list of available name attributes
Signature
GetAvailableAttributeNames()
Returns: Array of available attribute names. These names are specified in the customer defaults file. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableBeltSizes¶
-
ProfileBuilder.
GetAvailableBeltSizes
¶ Returns the list of available material attributes
Signature
GetAvailableBeltSizes()
Returns: Array of available belt types derived from the belt library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableBeltTypes¶
-
ProfileBuilder.
GetAvailableBeltTypes
¶ Returns the list of available material attributes
Signature
GetAvailableBeltTypes()
Returns: Array of available belt types derived from the belt library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableProfileSizes¶
-
ProfileBuilder.
GetAvailableProfileSizes
¶ Returns the list of available material attributes
Signature
GetAvailableProfileSizes()
Returns: Array of available profile types derived from the profile library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
GetAvailableProfileTypes¶
-
ProfileBuilder.
GetAvailableProfileTypes
¶ Returns the list of available material attributes
Signature
GetAvailableProfileTypes()
Returns: Array of available profile types derived from the profile library. :rtype: list of str
New in version NX7.5.0.
License requirements: None.
Validate¶
-
ProfileBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.