EndCutBlockBuilder Class¶
-
class
NXOpen.
EndCutBlockBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a End Cut Block Builder.
New in version NX5.3.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the angle |
Offset | Returns the offset |
SketchBlock | Returns the end cut block |
Tag | Returns the Tag for this object. |
TaperType | Returns or sets the taperType |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EndCutBlockBuilderTaperTypeOption Enumeration | Taper Type |
Property Detail¶
Angle¶
-
EndCutBlockBuilder.
Angle
¶ Returns the angle
-------------------------------------
Getter Method
Signature
Angle
Returns: Return type: NXOpen.Expression
New in version NX5.0.3.
License requirements: None.
Offset¶
-
EndCutBlockBuilder.
Offset
¶ Returns the offset
-------------------------------------
Getter Method
Signature
Offset
Returns: Return type: NXOpen.Expression
New in version NX5.0.3.
License requirements: None.
SketchBlock¶
-
EndCutBlockBuilder.
SketchBlock
¶ Returns the end cut block
-------------------------------------
Getter Method
Signature
SketchBlock
Returns: Return type: NXOpen.SketchExpressionModifierBuilder
New in version NX5.0.3.
License requirements: None.
TaperType¶
-
EndCutBlockBuilder.
TaperType
¶ Returns or sets the taperType
-------------------------------------
Getter Method
Signature
TaperType
Returns: Return type: NXOpen.EndCutBlockBuilderTaperTypeOption
New in version NX5.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaperType
Parameters: taperType ( NXOpen.EndCutBlockBuilderTaperTypeOption
) –New in version NX5.0.3.
License requirements: nx_ship_concept (“Ship Concept”)
Method Detail¶
Validate¶
-
EndCutBlockBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.