ProfileBuilderAlignment Enumeration¶
NXOpen.Features.ShipDesign.ProfileBuilder.Alignment is an alias for NXOpen.Features.ShipDesign.ProfileBuilderAlignment
-
class
NXOpen.Features.ShipDesign.
ProfileBuilderAlignment
¶ Bases:
object
Creation method used to define the placement of the belt this is disabled for profiles
Enum Members
Enum Member Enum Member Description Center GuideEdge OppositeGuide -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-