FlangeBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
FlangeBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Flange feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateFlangeFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BendAngle | Returns the bend angle for flange. |
BendOptions | Returns the bend options object. |
Edge | Returns or sets the edge on which the flange is created. |
FirstDistance | Returns a distance based on NXOpen.Features.SheetMetal.FlangeBuilder.WidthType() . |
InsetType | Returns or sets the inset type (inside, outside, bendoutside) for the flange. |
Length | Returns the length of the flange. |
LengthType | Returns or sets a enum indicating the length type. |
MatchFaceOption | Returns or sets the match face selection type. |
MatchPlane | Returns or sets the Match Plane. |
Offset | Returns the offset value for the flange. |
OffsetType | Returns or sets the offset type for the flange. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SecondDistance | Returns a distance based on NXOpen.Features.SheetMetal.FlangeBuilder.WidthType() . |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Vertex | Returns or sets the vertex on the flange edge, needed to dimension the flange width. |
WidthType | Returns or sets the width type for flange. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
DeleteSketch | Delete the flange sketch |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditSketch | Edit the sketch base on a new edge you need to call SetEdge to set a new edge |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetSketch | Get the flange sketch |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetBendAngle | |
SetFirstDistance | |
SetLength | |
SetOffset | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetSecondDistance | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify that the builder data is valid for creating a flange. |
Enumerations¶
FlangeBuilderInsetTypeOptions Enumeration | This enum represents the inset type for the material of the flange. |
FlangeBuilderLengthTypeOptions Enumeration | This enum indicates the two ways that the flange length can be measured. |
FlangeBuilderMatchFaceOptions Enumeration | This enum represents the match face option for the flange. |
FlangeBuilderOffsetTypeOptions Enumeration | This enum represents the offset type for the flange. |
FlangeBuilderWidthTypeOptions Enumeration | This enum represents the width type for the flange. |
Property Detail¶
BendAngle¶
-
FlangeBuilder.
BendAngle
¶ Returns the bend angle for flange.
It should be set in degrees (??????).
-------------------------------------
Getter Method
Signature
BendAngle
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
BendOptions¶
-
FlangeBuilder.
BendOptions
¶ Returns the bend options object.
The bend options object stores additional parameters for the bend, such as bend radius, bend relief width and depth, corner relief type etc.
-------------------------------------
Getter Method
Signature
BendOptions
Returns: Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Edge¶
-
FlangeBuilder.
Edge
¶ Returns or sets the edge on which the flange is created.
The edge should be linear and it should not be a thickness edge.
-------------------------------------
Getter Method
Signature
Edge
Returns: The flange is created on this edge. Return type: NXOpen.Edge
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
Edge
Parameters: edge ( NXOpen.Edge
) – The flange is created on this edge.New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
FirstDistance¶
-
FlangeBuilder.
FirstDistance
¶ Returns a distance based on
NXOpen.Features.SheetMetal.FlangeBuilder.WidthType()
.See
NXOpen.Features.SheetMetal.FlangeBuilder.WidthType`()
for a detailed desctiption of what this distance stands for.-------------------------------------
Getter Method
Signature
FirstDistance
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
InsetType¶
-
FlangeBuilder.
InsetType
¶ Returns or sets the inset type (inside, outside, bendoutside) for the flange.
-------------------------------------
Getter Method
Signature
InsetType
Returns: Return type: NXOpen.Features.SheetMetal.FlangeBuilderInsetTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
InsetType
Parameters: insetType ( NXOpen.Features.SheetMetal.FlangeBuilderInsetTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Length¶
-
FlangeBuilder.
Length
¶ Returns the length of the flange.
-------------------------------------
Getter Method
Signature
Length
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
LengthType¶
-
FlangeBuilder.
LengthType
¶ Returns or sets a enum indicating the length type.
For Features created in NX8 and above: The way length is measured for the flange. It can either be measure from the inside edge or the outside edge.
Flange length can be specified starting from the selected edge or from the corresponding edge on the other face (other linear edge on the other side of the thickness face). If the length is specified from the selected edge use value
NXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions.InsideDimension
or if the flange length is specifed from the other edge use valueNXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions.OutsideDimension
.For Features created in NX8 and above: Flange length can be measure from the Inner Mold Line, Outer Mold Line or Bend Tangent Line.
Inner Mold Line: Intersection of inner tab face and inner flange web face Outer Mold Line: Intersection of outer tab face and outer flange web face Bend Tangent Line: common edge between flange web face and bend face.
Flange length can be specified starting from the inner mold line or outer mold line or bend tangent line. If the length is specified from the inner mold line use value
NXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions.InsideDimension
or if the flange length is specifed from the outer mold line use valueNXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions.OutsideDimension
.-------------------------------------
Getter Method
Signature
LengthType
Returns: Return type: NXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
LengthType
Parameters: lengthType ( NXOpen.Features.SheetMetal.FlangeBuilderLengthTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
MatchFaceOption¶
-
FlangeBuilder.
MatchFaceOption
¶ Returns or sets the match face selection type.
None for Regular Flange. Until Selected for Match To Face type Flange .
-------------------------------------
Getter Method
Signature
MatchFaceOption
Returns: Return type: NXOpen.Features.SheetMetal.FlangeBuilderMatchFaceOptions
New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
MatchFaceOption
Parameters: matchFaceOption ( NXOpen.Features.SheetMetal.FlangeBuilderMatchFaceOptions
) –New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
MatchPlane¶
-
FlangeBuilder.
MatchPlane
¶ Returns or sets the Match Plane.
-------------------------------------
Getter Method
Signature
MatchPlane
Returns: Return type: NXOpen.Plane
New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
MatchPlane
Parameters: matchPlane ( NXOpen.Plane
) –New in version NX8.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Offset¶
-
FlangeBuilder.
Offset
¶ Returns the offset value for the flange.
-------------------------------------
Getter Method
Signature
Offset
Returns: The flange offset value Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
OffsetType¶
-
FlangeBuilder.
OffsetType
¶ Returns or sets the offset type for the flange.
-------------------------------------
Getter Method
Signature
OffsetType
Returns: The flange can be offset inside or outside. Return type: NXOpen.Features.SheetMetal.FlangeBuilderOffsetTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
OffsetType
Parameters: offsetType ( NXOpen.Features.SheetMetal.FlangeBuilderOffsetTypeOptions
) – The flange can be offset inside or outside.New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SecondDistance¶
-
FlangeBuilder.
SecondDistance
¶ Returns a distance based on
NXOpen.Features.SheetMetal.FlangeBuilder.WidthType()
.See
NXOpen.Features.SheetMetal.FlangeBuilder.WidthType`()
for a detailed desctiption of what this distance stands for.-------------------------------------
Getter Method
Signature
SecondDistance
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Vertex¶
-
FlangeBuilder.
Vertex
¶ Returns or sets the vertex on the flange edge, needed to dimension the flange width.
The vertex needs to be specified ONLY if
NXOpen.Features.SheetMetal.FlangeBuilder.WidthType()
is set to one ofNXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.AtEdgeEnd
,NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.FromEdgeEnd
. In case ofNXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.FromBothEnds
, the start vertex of the edge is assumed to be the start point forNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
.-------------------------------------
Getter Method
Signature
Vertex
Returns: A vertex on the flange edge. Return type: NXOpen.Point3d
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
Vertex
Parameters: vertex ( NXOpen.Point3d
) – A vertex on the flange edge.New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
WidthType¶
-
FlangeBuilder.
WidthType
¶ Returns or sets the width type for flange.
Use one of the values from
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions
. Depending on which of the values from the enum is used, none, either or both of the distance values fromNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
may be used. Here is a description of the distances:If the value is
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.FullEdge
, then both theFirstDistance()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
values are unused.If the value is
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.CenterOfEdge
, then both theNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
represent exactly half the width of the flange.If the value is
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.AtEdgeEnd
, thenNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
represents the width of the flange, starting from the end of the edge specified by theNXOpen.Features.SheetMetal.FlangeBuilder.Vertex()
and theNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
is not used.If the value is
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.FromEdgeEnd
, thenNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
represents the distance of the start point of the flange from the end of the edge specified byNXOpen.Features.SheetMetal.FlangeBuilder.Vertex()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
represents the width of the flange.If the value is
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.FromBothEnds
, thenNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
represents the distance of the start point of the flange from the from the end of the edge specified byNXOpen.Features.SheetMetal.FlangeBuilder.Vertex()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
represents the distance of the end point of the flange from end of the edge opposite to the end specified byNXOpen.Features.SheetMetal.FlangeBuilder.Vertex()
.The value
NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions.Custom
, cannot be set by the user. It is set internally if the sketch for the flange has been edited after creation. In this case, the expressionsNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
andNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
may or may not retain their original meaning when the flange was first created, so the user should not rely on these any more to mean anything specific.-------------------------------------
Getter Method
Signature
WidthType
Returns: Return type: NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
-------------------------------------
Setter Method
Signature
WidthType
Parameters: widthType ( NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions
) –New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Method Detail¶
DeleteSketch¶
-
FlangeBuilder.
DeleteSketch
¶ Delete the flange sketch
Signature
DeleteSketch()
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
EditSketch¶
-
FlangeBuilder.
EditSketch
¶ Edit the sketch base on a new edge you need to call SetEdge to set a new edge
Signature
EditSketch()
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
GetSketch¶
-
FlangeBuilder.
GetSketch
¶ Get the flange sketch
Signature
GetSketch()
Returns: Return type: NXOpen.Sketch
New in version NX6.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetBendAngle¶
-
FlangeBuilder.
SetBendAngle
¶ Signature
SetBendAngle(bendAngle)
Parameters: bendAngle (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.FlangeBuilder.BendAngle()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetFirstDistance¶
-
FlangeBuilder.
SetFirstDistance
¶ Signature
SetFirstDistance(firstDistance)
Parameters: firstDistance (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.FlangeBuilder.FirstDistance()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetLength¶
-
FlangeBuilder.
SetLength
¶ Signature
SetLength(length)
Parameters: length (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.FlangeBuilder.Length()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
SetOffset¶
-
FlangeBuilder.
SetOffset
¶ Signature
SetOffset(offset)
Parameters: offset (str) – The flange offset value New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.FlangeBuilder.Offset()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetSecondDistance¶
-
FlangeBuilder.
SetSecondDistance
¶ Signature
SetSecondDistance(secondDistance)
Parameters: secondDistance (str) – New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.FlangeBuilder.SecondDistance()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
FlangeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
FlangeBuilder.
ValidateBuilderData
¶ Verify that the builder data is valid for creating a flange.
If the builder data is valid, return value is zero.
Signature
ValidateBuilderData()
Returns: A value of zero is returned if the data in the builder is valid. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)