FlangeBuilderInsetTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.FlangeBuilder.InsetTypeOptions is an alias for NXOpen.Features.SheetMetal.FlangeBuilderInsetTypeOptions
-
class
NXOpen.Features.SheetMetal.
FlangeBuilderInsetTypeOptions
¶ Bases:
object
This enum represents the inset type for the material of the flange.
Enum Members
Enum Member Enum Member Description MaterialInside The flange is flush with the thickness face on the inside MaterialOutside The flange is flush with the thickness face on the outside BendOutside The bend and flange are outside the thickness face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-