FlangeBuilderWidthTypeOptions Enumeration¶
NXOpen.Features.SheetMetal.FlangeBuilder.WidthTypeOptions is an alias for NXOpen.Features.SheetMetal.FlangeBuilderWidthTypeOptions
-
class
NXOpen.Features.SheetMetal.
FlangeBuilderWidthTypeOptions
¶ Bases:
object
This enum represents the width type for the flange.
Enum Members
Enum Member Enum Member Description FullEdge The flange spans the entire edge. CenterOfEdge The flange is centered on the edge. AtEdgeEnd The flange starts from the specified end of the edge. FromEdgeEnd The flange starts at a specified distance from an end of the edge. FromBothEnds The flange starts and ends at specified distances from the ends of the edge. Custom The flange sketch has been edited after creation and may or may not conform to any of the above. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-