FlangeBuilderMatchFaceOptions Enumeration¶
NXOpen.Features.SheetMetal.FlangeBuilder.MatchFaceOptions is an alias for NXOpen.Features.SheetMetal.FlangeBuilderMatchFaceOptions
-
class
NXOpen.Features.SheetMetal.
FlangeBuilderMatchFaceOptions
¶ Bases:
object
This enum represents the match face option for the flange.
Enum Members
Enum Member Enum Member Description NotSet The flange is placed on the selected edge UntilSelected The flange face is extended until the selected plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-