PoleSmoothingBuilder Class¶
-
class
NXOpen.Features.
PoleSmoothingBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.PoleSmoothing
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreatePoleSmoothingBuilder()
Default values.
Property Value ApplyConstraintsToAll 0 ModificationPercentage 100 MoveOnlySelectedPoles 0 SmoothingFactor 1 UseSpecificDirection 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ApplyConstraintsToAll | Returns or sets the indicator to apply the same constraint to all |
ModificationPercentage | Returns or sets the modification percentage |
MoveOnlySelectedPoles | Returns or sets the indicator to move only selected poles |
MovementVector | Returns or sets the movement direction vector, this is used only when UseSpecificDirection`() is true. |
NumberPolesSelected | Returns or sets the number of poles selected |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Poles | Returns the selected poles, this is used only when MoveOnlySelectedPoles`() is true |
SmoothingFactor | Returns or sets the smoothing factor, the min and max values for this are (1 to 100) |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face |
UMaxConstraint | Returns the u maximum continuity constraint |
UMinConstraint | Returns the u minimum continuity constraint |
UseSpecificDirection | Returns or sets the specific moving direction |
VMaxConstraint | Returns the v maximum continuity constraint |
VMinConstraint | Returns the v minimum continuity constraint |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCreateNewCopy | Returns the indicator for creating a new copy |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetSelectedPolesIndex | Returns the index of selected poles |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveFeatureParameters | Removes parameters of a owning feature of a face to be smoothed |
SetCreateNewCopy | Sets the indicator for creating a new copy |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetSelectedPolesIndex | Sets the index of selected poles |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ApplyConstraintsToAll¶
-
PoleSmoothingBuilder.
ApplyConstraintsToAll
¶ Returns or sets the indicator to apply the same constraint to all
-------------------------------------
Getter Method
Signature
ApplyConstraintsToAll
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
ApplyConstraintsToAll
Parameters: applyConstraintsToAll (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
ModificationPercentage¶
-
PoleSmoothingBuilder.
ModificationPercentage
¶ Returns or sets the modification percentage
-------------------------------------
Getter Method
Signature
ModificationPercentage
Returns: Return type: int New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
ModificationPercentage
Parameters: modificationPercentage (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
MoveOnlySelectedPoles¶
-
PoleSmoothingBuilder.
MoveOnlySelectedPoles
¶ Returns or sets the indicator to move only selected poles
-------------------------------------
Getter Method
Signature
MoveOnlySelectedPoles
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
MoveOnlySelectedPoles
Parameters: moveOnlySelectedPoles (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
MovementVector¶
-
PoleSmoothingBuilder.
MovementVector
¶ Returns or sets the movement direction vector, this is used only when
UseSpecificDirection`()
is true.-------------------------------------
Getter Method
Signature
MovementVector
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
MovementVector
Parameters: movementVector ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
NumberPolesSelected¶
-
PoleSmoothingBuilder.
NumberPolesSelected
¶ Returns or sets the number of poles selected
-------------------------------------
Getter Method
Signature
NumberPolesSelected
Returns: Return type: int New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
NumberPolesSelected
Parameters: numbePolesSelected (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Poles¶
-
PoleSmoothingBuilder.
Poles
¶ Returns the selected poles, this is used only when
MoveOnlySelectedPoles`()
is true-------------------------------------
Getter Method
Signature
Poles
Returns: Return type: NXOpen.GeometricUtilities.ControlPoleManagerData
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SmoothingFactor¶
-
PoleSmoothingBuilder.
SmoothingFactor
¶ Returns or sets the smoothing factor, the min and max values for this are (1 to 100)
-------------------------------------
Getter Method
Signature
SmoothingFactor
Returns: Return type: int New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
SmoothingFactor
Parameters: smoothingFactor (int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
TargetFace¶
-
PoleSmoothingBuilder.
TargetFace
¶ Returns the target face
-------------------------------------
Getter Method
Signature
TargetFace
Returns: Return type: NXOpen.SelectFace
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
UMaxConstraint¶
-
PoleSmoothingBuilder.
UMaxConstraint
¶ Returns the u maximum continuity constraint
-------------------------------------
Getter Method
Signature
UMaxConstraint
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
UMinConstraint¶
-
PoleSmoothingBuilder.
UMinConstraint
¶ Returns the u minimum continuity constraint
-------------------------------------
Getter Method
Signature
UMinConstraint
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
UseSpecificDirection¶
-
PoleSmoothingBuilder.
UseSpecificDirection
¶ Returns or sets the specific moving direction
-------------------------------------
Getter Method
Signature
UseSpecificDirection
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
UseSpecificDirection
Parameters: useSpecificDirection (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
VMaxConstraint¶
-
PoleSmoothingBuilder.
VMaxConstraint
¶ Returns the v maximum continuity constraint
-------------------------------------
Getter Method
Signature
VMaxConstraint
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
VMinConstraint¶
-
PoleSmoothingBuilder.
VMinConstraint
¶ Returns the v minimum continuity constraint
-------------------------------------
Getter Method
Signature
VMinConstraint
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
GetCreateNewCopy¶
-
PoleSmoothingBuilder.
GetCreateNewCopy
¶ Returns the indicator for creating a new copy
Signature
GetCreateNewCopy()
Returns: Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
GetSelectedPolesIndex¶
-
PoleSmoothingBuilder.
GetSelectedPolesIndex
¶ Returns the index of selected poles
Signature
GetSelectedPolesIndex()
Returns: Return type: list of int New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
RemoveFeatureParameters¶
-
PoleSmoothingBuilder.
RemoveFeatureParameters
¶ Removes parameters of a owning feature of a face to be smoothed
Signature
RemoveFeatureParameters(face)
Parameters: face ( NXOpen.Face
) – Face to be used for feature parameter removalNew in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SetCreateNewCopy¶
-
PoleSmoothingBuilder.
SetCreateNewCopy
¶ Sets the indicator for creating a new copy
Signature
SetCreateNewCopy(createNewCopy)
Parameters: createNewCopy (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
SetSelectedPolesIndex¶
-
PoleSmoothingBuilder.
SetSelectedPolesIndex
¶ Sets the index of selected poles
Signature
SetSelectedPolesIndex(selectedPolesIndex)
Parameters: selectedPolesIndex (list of int) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
PoleSmoothingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.