ControlPoleManagerData Class¶
-
class
NXOpen.GeometricUtilities.
ControlPoleManagerData
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class manages the control poles for a set of surfaces or curves.
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePolesGroup | Creates a new poles group |
DeletePolesGroup | Deletes a group of poles |
DeselectPoles | Removes selected pole |
GetIsUPeriodic | Queries periodicity in U direction of a group of poles |
GetIsVPeriodic | Queries periodicity in V direction of a group of poles |
GetPoles | Gets poles of an entity |
GetSelectedPoles | Gets selected poles |
GetUDimension | Queries dimension in U direction of a group of poles |
GetVDimension | Queries dimension in V direction of a group of poles |
SelectPoles | Adds new selected pole |
SetIsUPeriodic | Sets periodicity in U direction of a group of poles |
SetIsVPeriodic | Sets periodicity in V direction of a group of poles |
SetPoleGroupEntity | Sets face to control poles group |
SetPoles | Sets new group poles |
SetUDimension | Sets dimension in U direction of a group of poles |
SetVDimension | Sets dimension in V direction of a group of poles |
UpdatePolePositions | Updates pole positions |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
CreatePolesGroup¶
-
ControlPoleManagerData.
CreatePolesGroup
¶ Creates a new poles group
Signature
CreatePolesGroup()
Returns: New group index for newly created poles group. Return type: int New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DeletePolesGroup¶
-
ControlPoleManagerData.
DeletePolesGroup
¶ Deletes a group of poles
Signature
DeletePolesGroup(groupIndex)
Parameters: groupIndex (int) – Group index for the group to be deleted. New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
DeselectPoles¶
-
ControlPoleManagerData.
DeselectPoles
¶ Removes selected pole
Signature
DeselectPoles(groupIndex, polesIndex, poles)
Parameters: - groupIndex (int) – Entity group index. Control Pole Manager needs to handle poles from different surfaces or curves. Therefore, poles need to be grouped. Poles associated with the same entity are placed into a group. When setting or getting poles from the Pole Manager, the caller needs to provide a group index to identify poles with the proper entity group.
- polesIndex (list of int) – Poles index
- poles (list of
NXOpen.Point
) – Poles
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetIsUPeriodic¶
-
ControlPoleManagerData.
GetIsUPeriodic
¶ Queries periodicity in U direction of a group of poles
Signature
GetIsUPeriodic(groupIndex)
Parameters: groupIndex (int) – poles group index Returns: U Periodicity Return type: bool New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetIsVPeriodic¶
-
ControlPoleManagerData.
GetIsVPeriodic
¶ Queries periodicity in V direction of a group of poles
Signature
GetIsVPeriodic(groupIndex)
Parameters: groupIndex (int) – poles group index Returns: V Periodicity Return type: bool New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetPoles¶
-
ControlPoleManagerData.
GetPoles
¶ Gets poles of an entity
Signature
GetPoles(groupIndex)
Parameters: groupIndex (int) – Entity group index. Control Pole Manager needs to handle poles from different surfaces or curves. Therefore, poles need to be grouped. Poles associated with the same entity are placed into a group. When setting or getting poles from the Pole Manager, the caller needs to provide a group index to identify poles with the proper entity group. Returns: a tuple Return type: A tuple consisting of (polesIndex, poles). polesIndex is a list of int. Poles index poles is a list of NXOpen.Point
. PolesNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetSelectedPoles¶
-
ControlPoleManagerData.
GetSelectedPoles
¶ Gets selected poles
Signature
GetSelectedPoles(groupIndex)
Parameters: groupIndex (int) – Entity group index. Control Pole Manager needs to handle poles from different surfaces or curves. Therefore, poles need to be grouped. Poles associated with the same entity are placed into a group. When setting or getting poles from the Pole Manager, the caller needs to provide a group index to identify poles with the proper entity group. Returns: a tuple Return type: A tuple consisting of (polesIndex, poles). polesIndex is a list of int. Poles index poles is a list of NXOpen.Point
. PolesNew in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetUDimension¶
-
ControlPoleManagerData.
GetUDimension
¶ Queries dimension in U direction of a group of poles
Signature
GetUDimension(groupIndex)
Parameters: groupIndex (int) – poles group index Returns: U Dimension Return type: int New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
GetVDimension¶
-
ControlPoleManagerData.
GetVDimension
¶ Queries dimension in V direction of a group of poles
Signature
GetVDimension(groupIndex)
Parameters: groupIndex (int) – poles group index Returns: V Dimension Return type: int New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SelectPoles¶
-
ControlPoleManagerData.
SelectPoles
¶ Adds new selected pole
Signature
SelectPoles(groupIndex, polesIndex, poles)
Parameters: - groupIndex (int) – Entity group index. Control Pole Manager needs to handle poles from different surfaces or curves. Therefore, poles need to be grouped. Poles associated with the same entity are placed into a group. When setting or getting poles from the Pole Manager, the caller needs to provide a group index to identify poles with the proper entity group.
- polesIndex (list of int) – Poles index
- poles (list of
NXOpen.Point
) – Poles
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetIsUPeriodic¶
-
ControlPoleManagerData.
SetIsUPeriodic
¶ Sets periodicity in U direction of a group of poles
Signature
SetIsUPeriodic(groupIndex, uPeriodicity)
Parameters: - groupIndex (int) – poles group index
- uPeriodicity (bool) – U Periodicity
New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetIsVPeriodic¶
-
ControlPoleManagerData.
SetIsVPeriodic
¶ Sets periodicity in V direction of a group of poles
Signature
SetIsVPeriodic(groupIndex, vPeriodicity)
Parameters: - groupIndex (int) – poles group index
- vPeriodicity (bool) – V Periodicity
New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetPoleGroupEntity¶
-
ControlPoleManagerData.
SetPoleGroupEntity
¶ Overloaded method SetPoleGroupEntity
SetPoleGroupEntity(groupIndex, face)
SetPoleGroupEntity(groupIndex, curve)
-------------------------------------
Sets face to control poles group
Signature
SetPoleGroupEntity(groupIndex, face)
Parameters: - groupIndex (int) – pole group index
- face (
NXOpen.Face
) – face
New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Sets curve to control poles group
Signature
SetPoleGroupEntity(groupIndex, curve)
Parameters: - groupIndex (int) – pole group index
- curve (
NXOpen.Curve
) – curve
New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
SetPoles¶
-
ControlPoleManagerData.
SetPoles
¶ Sets new group poles
Signature
SetPoles(groupIndex, polesIndex, poles)
Parameters: - groupIndex (int) – Entity group index. Control Pole Manager needs to handle poles from different surfaces or curves. Therefore, poles need to be grouped. Poles associated with the same entity are placed into a group. When setting or getting poles from the Pole Manager, the caller needs to provide a group index to identify poles with the proper entity group.
- polesIndex (list of int) – Poles index
- poles (list of
NXOpen.Point
) – Poles
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetUDimension¶
-
ControlPoleManagerData.
SetUDimension
¶ Sets dimension in U direction of a group of poles
Signature
SetUDimension(groupIndex, uDimension)
Parameters: - groupIndex (int) – poles group index
- uDimension (int) – U Dimension
New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetVDimension¶
-
ControlPoleManagerData.
SetVDimension
¶ Sets dimension in V direction of a group of poles
Signature
SetVDimension(groupIndex, vDimension)
Parameters: - groupIndex (int) – poles group index
- vDimension (int) – V Dimension
New in version NX6.0.1.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UpdatePolePositions¶
-
ControlPoleManagerData.
UpdatePolePositions
¶ Updates pole positions
Signature
UpdatePolePositions(groupIndex, poleIndex, newPosition)
Parameters: - groupIndex (int) – poles group index
- poleIndex (list of int) – pole index in the group
- newPosition (list of
NXOpen.Point3d
) – Pole new position
New in version NX7.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
ControlPoleManagerData.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.