OffsetEdgeBuilder Class¶
-
class
NXOpen.Features.
OffsetEdgeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.OffsetEdge
builderTo create a new instance of this class, use
NXOpen.Features.SynchronousEdgeCollection.CreateOffsetEdgeBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns the distance for offset edge |
EdgeToOffset | Returns the edge collector to offset |
EndFaceBehavior | Returns or sets whether fix side faces |
Method | Returns or sets the method for offset edge |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReverseOffsetDirection | Returns or sets whether reverse offset direction |
ReverseOffsetSide | Returns or sets whether reverse offset side |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OffsetEdgeBuilderEndFaceBehaviourType Enumeration | the end face behavior settings enumeration |
OffsetEdgeBuilderOffsetEdgeMethod Enumeration | the offset edge method enumeration |
Property Detail¶
Distance¶
-
OffsetEdgeBuilder.
Distance
¶ Returns the distance for offset edge
-------------------------------------
Getter Method
Signature
Distance
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
EdgeToOffset¶
-
OffsetEdgeBuilder.
EdgeToOffset
¶ Returns the edge collector to offset
-------------------------------------
Getter Method
Signature
EdgeToOffset
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
EndFaceBehavior¶
-
OffsetEdgeBuilder.
EndFaceBehavior
¶ Returns or sets whether fix side faces
-------------------------------------
Getter Method
Signature
EndFaceBehavior
Returns: Return type: NXOpen.Features.OffsetEdgeBuilderEndFaceBehaviourType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndFaceBehavior
Parameters: endFaceBehaviour ( NXOpen.Features.OffsetEdgeBuilderEndFaceBehaviourType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method¶
-
OffsetEdgeBuilder.
Method
¶ Returns or sets the method for offset edge
-------------------------------------
Getter Method
Signature
Method
Returns: Return type: NXOpen.Features.OffsetEdgeBuilderOffsetEdgeMethod
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Method
Parameters: method ( NXOpen.Features.OffsetEdgeBuilderOffsetEdgeMethod
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReverseOffsetDirection¶
-
OffsetEdgeBuilder.
ReverseOffsetDirection
¶ Returns or sets whether reverse offset direction
-------------------------------------
Getter Method
Signature
ReverseOffsetDirection
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseOffsetDirection
Parameters: reverseOffsetDirection (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReverseOffsetSide¶
-
OffsetEdgeBuilder.
ReverseOffsetSide
¶ Returns or sets whether reverse offset side
-------------------------------------
Getter Method
Signature
ReverseOffsetSide
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseOffsetSide
Parameters: reverseOffsetSide (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
OffsetEdgeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.