OffsetEdgeBuilderOffsetEdgeMethod Enumeration

NXOpen.Features.OffsetEdgeBuilder.OffsetEdgeMethod is an alias for NXOpen.Features.OffsetEdgeBuilderOffsetEdgeMethod

class NXOpen.Features.OffsetEdgeBuilderOffsetEdgeMethod

Bases: object

the offset edge method enumeration

Enum Members

Enum Member Enum Member Description
AlongFace
AlongPlaneofEdge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.