OffsetEdgeBuilderEndFaceBehaviourType Enumeration

NXOpen.Features.OffsetEdgeBuilder.EndFaceBehaviourType is an alias for NXOpen.Features.OffsetEdgeBuilderEndFaceBehaviourType

class NXOpen.Features.OffsetEdgeBuilderEndFaceBehaviourType

Bases: object

the end face behavior settings enumeration

Enum Members

Enum Member Enum Member Description
Extend
Morph
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.