InspectionToleranceOperationBuilder Class¶
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
this class creates the tolerance operation
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionToleranceOperationBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CompositeToleranceValueSource | Returns or sets the GDT Composite Lower Tolerance Value Source |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DatumPlaneFittingModeBuilder | Returns the Datum Plane Fitting Mode Builder |
Description | Returns or sets the description |
DirVec | Returns or sets the selected vector for tolerance direction |
DofCsysMode | Returns or sets the Degree of Freedom Coordinate System Mode |
DoubleDirVecI | Returns or sets the double dir vec i |
DoubleDirVecJ | Returns or sets the double dir vec j |
DoubleDirVecK | Returns or sets the double dir vec k |
DoubleLower | Returns or sets the lower tolerance |
DoubleLowerParamOuterProfile | Returns or sets the double lower parameter outer profile |
DoubleNominal | Returns or sets the nominal tolerance |
DoubleParamExtArea | Returns or sets the double parameter extent area |
DoubleParamExtLength | Returns or sets the double parameter extent length |
DoubleParamOuterProfile | Returns or sets the double parameter outer profile |
DoubleParamTolValue | Returns or sets the double parameter tolerance value |
DoubleParamTolValue1 | Returns or sets the double parameter tolerance value1 |
DoubleUpper | Returns or sets the upper tolerance |
DoubleViewVecI | Returns or sets the double view vec i |
DoubleViewVecJ | Returns or sets the double view vec j |
DoubleViewVecK | Returns or sets the double view vec k |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
EnumPCSABS | Returns or sets the enum pcsabs |
EnumParamPriMatModifier | Returns or sets the enum parameter primary material modifier |
EnumParamPriMatModifier1 | Returns or sets the enum parameter primary material modifier1 |
EnumParamSecMatModifier | Returns or sets the enum parameter secondary material modifier |
EnumParamSecMatModifier1 | Returns or sets the enum parameter secondary material modifier1 |
EnumParamSubType | Returns or sets the enum parameter sub type |
EnumParamTerMatModifier | Returns or sets the enum parameter tertiary material modifier |
EnumParamTerMatModifier1 | Returns or sets the enum parameter tertiary material modifier1 |
EnumParamTolMatModifier | Returns or sets the enum parameter tolerance material modifier |
EnumParamTolMatModifier1 | Returns or sets the enum parameter tolerance material modifier1 |
EnumParamTolMatModifierDup | Returns or sets the enum parameter tolerance material modifier dup |
EnumParamTolZoneShape | Returns or sets the enum parameter tolerance zone shape |
EnumParamTolZoneShape1 | Returns or sets the enum parameter tolerance zone shape1 |
EnumParamXYZAxis | Returns or sets the enum parameter xyzaxis |
EnumParameterExtent | Returns or sets the enum parameter extent |
EnumTorusCharacteristic | Returns or sets the enum torus characteristic |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IsAlignVector | Returns or sets the is Align Vector Flag |
IsComposite | Returns or sets the is composite flag |
LayoutAndLayer | Returns the Layer and Layout |
LimitsOfSizeModeBuilder | Returns the Limits of Size Mode Builder |
LowerDMS | Returns or sets the string for anglb upper DMS |
LowerSource | Returns or sets the Lower Value Source |
MotionOutputBuilder | Returns the motion output builder |
NominalDMS | Returns or sets the string for anglb nominal DMS |
NominalSource | Returns or sets the Nominal Value Source |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ProfileDispositionModeBuilder | Returns the Profile Disposition Mode Builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectionFeature | Returns the selection feature |
SelectionOriginFeature | Returns the selection origin feature |
SelectionPMI | Returns the PMI selection |
SelectionTolerancedFeature | Returns the selection toleranced feature |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
StringDatumFeatName | Returns or sets the string datum feat name |
StringDatumLetter | Returns or sets the string datum letter |
StringOriginFeatName | Returns or sets the string origin feat name |
StringPriDatum | Returns or sets the string primary datum |
StringPriDatum1 | Returns or sets the string primary datum1 |
StringSecDatum | Returns or sets the string secondary datum |
StringSecDatum1 | Returns or sets the string secondary datum1 |
StringTerDatum | Returns or sets the string tertiary datum |
StringTerDatum1 | Returns or sets the string tertiary datum1 |
StringTolName | Returns or sets the string tolerance name |
StringTolerancedFeat | Returns or sets the string toleranced feat |
SurfaceProfileModeBuilder | Returns the Surface Profile Mode Builder |
Tag | Returns the Tag for this object. |
TolOpType | Returns or sets the tolerance type |
ToleranceValueSource | Returns or sets the GDT Tolerance Value Source |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
UpperDMS | Returns or sets the string for anglb upper DMS |
UpperSource | Returns or sets the Upper Value Source |
UseDegMin | Returns or sets the deg/min flag for angle between |
VectorDirection | Returns or sets the vector direction |
VectorViewVec | Returns or sets the vector view vec |
XRotationDOFMode | Returns or sets the x rotation dofmode |
XRotationLowerLimit | Returns or sets the x rotation lower limit |
XRotationUpperLimit | Returns or sets the x rotation upper limit |
XTranslationDOFMode | Returns or sets the x translation dofmode |
XTranslationLowerLimit | Returns or sets the x translation lower limit |
XTranslationUpperLimit | Returns or sets the x translation upper limit |
YRotationDOFMode | Returns or sets the y rotation dofmode |
YRotationLowerLimit | Returns or sets the y rotation lower limit |
YRotationUpperLimit | Returns or sets the y rotation upper limit |
YTranslationDOFMode | Returns or sets the y translation dofmode |
YTranslationLowerLimit | Returns or sets the y translation lower limit |
YTranslationUpperLimit | Returns or sets the y translation upper limit |
ZRotationDOFMode | Returns or sets the z rotation dofmode |
ZRotationLowerLimit | Returns or sets the z rotation lower limit |
ZRotationUpperLimit | Returns or sets the z rotation upper limit |
ZTranslationDOFMode | Returns or sets the z translation dofmode |
ZTranslationLowerLimit | Returns or sets the z translation lower limit |
ZTranslationUpperLimit | Returns or sets the z translation upper limit |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParameters | Updates Inspection tolerance parameters based on selected annotation. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
CompositeToleranceValueSource¶
-
InspectionToleranceOperationBuilder.
CompositeToleranceValueSource
¶ Returns or sets the GDT Composite Lower Tolerance Value Source
-------------------------------------
Getter Method
Signature
CompositeToleranceValueSource
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompositeToleranceValueSource
Parameters: compositeToleranceValueSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DatumPlaneFittingModeBuilder¶
-
InspectionToleranceOperationBuilder.
DatumPlaneFittingModeBuilder
¶ Returns the Datum Plane Fitting Mode Builder
-------------------------------------
Getter Method
Signature
DatumPlaneFittingModeBuilder
Returns: Return type: NXOpen.CAM.InspectionDatumPlaneFittingModeBuilder
New in version NX9.0.0.
License requirements: None.
DirVec¶
-
InspectionToleranceOperationBuilder.
DirVec
¶ Returns or sets the selected vector for tolerance direction
-------------------------------------
Getter Method
Signature
DirVec
Returns: Return type: NXOpen.Direction
New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirVec
Parameters: dirVec ( NXOpen.Direction
) –New in version NX10.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DofCsysMode¶
-
InspectionToleranceOperationBuilder.
DofCsysMode
¶ Returns or sets the Degree of Freedom Coordinate System Mode
-------------------------------------
Getter Method
Signature
DofCsysMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomCsysMode
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
DofCsysMode
Parameters: dofCsysMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomCsysMode
) –New in version NX9.0.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleDirVecI¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecI
¶ Returns or sets the double dir vec i
-------------------------------------
Getter Method
Signature
DoubleDirVecI
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecI
Parameters: doubleDirVecI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleDirVecJ¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecJ
¶ Returns or sets the double dir vec j
-------------------------------------
Getter Method
Signature
DoubleDirVecJ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecJ
Parameters: doubleDirVecJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleDirVecK¶
-
InspectionToleranceOperationBuilder.
DoubleDirVecK
¶ Returns or sets the double dir vec k
-------------------------------------
Getter Method
Signature
DoubleDirVecK
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleDirVecK
Parameters: doubleDirVecK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleLower¶
-
InspectionToleranceOperationBuilder.
DoubleLower
¶ Returns or sets the lower tolerance
-------------------------------------
Getter Method
Signature
DoubleLower
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleLower
Parameters: doubleLower (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleLowerParamOuterProfile¶
-
InspectionToleranceOperationBuilder.
DoubleLowerParamOuterProfile
¶ Returns or sets the double lower parameter outer profile
-------------------------------------
Getter Method
Signature
DoubleLowerParamOuterProfile
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleLowerParamOuterProfile
Parameters: doubleLowerParamOuterProfile (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleNominal¶
-
InspectionToleranceOperationBuilder.
DoubleNominal
¶ Returns or sets the nominal tolerance
-------------------------------------
Getter Method
Signature
DoubleNominal
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleNominal
Parameters: doubleNominal (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamExtArea¶
-
InspectionToleranceOperationBuilder.
DoubleParamExtArea
¶ Returns or sets the double parameter extent area
-------------------------------------
Getter Method
Signature
DoubleParamExtArea
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamExtArea
Parameters: doubleParamExtArea (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamExtLength¶
-
InspectionToleranceOperationBuilder.
DoubleParamExtLength
¶ Returns or sets the double parameter extent length
-------------------------------------
Getter Method
Signature
DoubleParamExtLength
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamExtLength
Parameters: doubleParamExtLength (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamOuterProfile¶
-
InspectionToleranceOperationBuilder.
DoubleParamOuterProfile
¶ Returns or sets the double parameter outer profile
-------------------------------------
Getter Method
Signature
DoubleParamOuterProfile
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamOuterProfile
Parameters: doubleParamOuterProfile (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamTolValue¶
-
InspectionToleranceOperationBuilder.
DoubleParamTolValue
¶ Returns or sets the double parameter tolerance value
-------------------------------------
Getter Method
Signature
DoubleParamTolValue
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamTolValue
Parameters: doubleParamTolValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleParamTolValue1¶
-
InspectionToleranceOperationBuilder.
DoubleParamTolValue1
¶ Returns or sets the double parameter tolerance value1
-------------------------------------
Getter Method
Signature
DoubleParamTolValue1
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleParamTolValue1
Parameters: doubleParamTolValue1 (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleUpper¶
-
InspectionToleranceOperationBuilder.
DoubleUpper
¶ Returns or sets the upper tolerance
-------------------------------------
Getter Method
Signature
DoubleUpper
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleUpper
Parameters: doubleUpper (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecI¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecI
¶ Returns or sets the double view vec i
-------------------------------------
Getter Method
Signature
DoubleViewVecI
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecI
Parameters: doubleViewVecI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecJ¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecJ
¶ Returns or sets the double view vec j
-------------------------------------
Getter Method
Signature
DoubleViewVecJ
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecJ
Parameters: doubleViewVecJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DoubleViewVecK¶
-
InspectionToleranceOperationBuilder.
DoubleViewVecK
¶ Returns or sets the double view vec k
-------------------------------------
Getter Method
Signature
DoubleViewVecK
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DoubleViewVecK
Parameters: doubleViewVecK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumPCSABS¶
-
InspectionToleranceOperationBuilder.
EnumPCSABS
¶ Returns or sets the enum pcsabs
-------------------------------------
Getter Method
Signature
EnumPCSABS
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderSirVecPCSABS
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumPCSABS
Parameters: enumPCSABS ( NXOpen.CAM.InspectionToleranceOperationBuilderSirVecPCSABS
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamPriMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamPriMatModifier
¶ Returns or sets the enum parameter primary material modifier
-------------------------------------
Getter Method
Signature
EnumParamPriMatModifier
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamPriMatModifier
Parameters: enumParamPriMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamPriMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamPriMatModifier1
¶ Returns or sets the enum parameter primary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamPriMatModifier1
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamPriMatModifier1
Parameters: enumParamPriMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSecMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamSecMatModifier
¶ Returns or sets the enum parameter secondary material modifier
-------------------------------------
Getter Method
Signature
EnumParamSecMatModifier
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSecMatModifier
Parameters: enumParamSecMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSecMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamSecMatModifier1
¶ Returns or sets the enum parameter secondary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamSecMatModifier1
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSecMatModifier1
Parameters: enumParamSecMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSecDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamSubType¶
-
InspectionToleranceOperationBuilder.
EnumParamSubType
¶ Returns or sets the enum parameter sub type
-------------------------------------
Getter Method
Signature
EnumParamSubType
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamSubType
Parameters: enumParamSubType ( NXOpen.CAM.InspectionToleranceOperationBuilderParamSubType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTerMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamTerMatModifier
¶ Returns or sets the enum parameter tertiary material modifier
-------------------------------------
Getter Method
Signature
EnumParamTerMatModifier
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTerMatModifier
Parameters: enumParamTerMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTerMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamTerMatModifier1
¶ Returns or sets the enum parameter tertiary material modifier1
-------------------------------------
Getter Method
Signature
EnumParamTerMatModifier1
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTerMatModifier1
Parameters: enumParamTerMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTerDatumModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifier¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifier
¶ Returns or sets the enum parameter tolerance material modifier
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifier
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifier
Parameters: enumParamTolMatModifier ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifier1¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifier1
¶ Returns or sets the enum parameter tolerance material modifier1
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifier1
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifier1
Parameters: enumParamTolMatModifier1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifier
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolMatModifierDup¶
-
InspectionToleranceOperationBuilder.
EnumParamTolMatModifierDup
¶ Returns or sets the enum parameter tolerance material modifier dup
-------------------------------------
Getter Method
Signature
EnumParamTolMatModifierDup
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifierDup
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolMatModifierDup
Parameters: enumParamTolMatModifierDup ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolMatModifierDup
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolZoneShape¶
-
InspectionToleranceOperationBuilder.
EnumParamTolZoneShape
¶ Returns or sets the enum parameter tolerance zone shape
-------------------------------------
Getter Method
Signature
EnumParamTolZoneShape
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolZoneShape
Parameters: enumParamTolZoneShape ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamTolZoneShape1¶
-
InspectionToleranceOperationBuilder.
EnumParamTolZoneShape1
¶ Returns or sets the enum parameter tolerance zone shape1
-------------------------------------
Getter Method
Signature
EnumParamTolZoneShape1
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamTolZoneShape1
Parameters: enumParamTolZoneShape1 ( NXOpen.CAM.InspectionToleranceOperationBuilderParamTolZoneShape
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParamXYZAxis¶
-
InspectionToleranceOperationBuilder.
EnumParamXYZAxis
¶ Returns or sets the enum parameter xyzaxis
-------------------------------------
Getter Method
Signature
EnumParamXYZAxis
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParamXYZAxis
Parameters: enumParamXYZAxis ( NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumParameterExtent¶
-
InspectionToleranceOperationBuilder.
EnumParameterExtent
¶ Returns or sets the enum parameter extent
-------------------------------------
Getter Method
Signature
EnumParameterExtent
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamExtent
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumParameterExtent
Parameters: enumParameterExtent ( NXOpen.CAM.InspectionToleranceOperationBuilderParamExtent
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EnumTorusCharacteristic¶
-
InspectionToleranceOperationBuilder.
EnumTorusCharacteristic
¶ Returns or sets the enum torus characteristic
-------------------------------------
Getter Method
Signature
EnumTorusCharacteristic
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnumTorusCharacteristic
Parameters: enumTorusCharacteristic ( NXOpen.CAM.InspectionToleranceOperationBuilderParamXYZAxis
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsAlignVector¶
-
InspectionToleranceOperationBuilder.
IsAlignVector
¶ Returns or sets the is Align Vector Flag
-------------------------------------
Getter Method
Signature
IsAlignVector
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsAlignVector
Parameters: isAlignVector (bool) – New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsComposite¶
-
InspectionToleranceOperationBuilder.
IsComposite
¶ Returns or sets the is composite flag
-------------------------------------
Getter Method
Signature
IsComposite
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsComposite
Parameters: isComposite (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LimitsOfSizeModeBuilder¶
-
InspectionToleranceOperationBuilder.
LimitsOfSizeModeBuilder
¶ Returns the Limits of Size Mode Builder
-------------------------------------
Getter Method
Signature
LimitsOfSizeModeBuilder
Returns: Return type: NXOpen.CAM.InspectionLimitsOfSizeModeBuilder
New in version NX9.0.0.
License requirements: None.
LowerDMS¶
-
InspectionToleranceOperationBuilder.
LowerDMS
¶ Returns or sets the string for anglb upper DMS
-------------------------------------
Getter Method
Signature
LowerDMS
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerDMS
Parameters: stringLowerDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LowerSource¶
-
InspectionToleranceOperationBuilder.
LowerSource
¶ Returns or sets the Lower Value Source
-------------------------------------
Getter Method
Signature
LowerSource
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerSource
Parameters: lowerSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NominalDMS¶
-
InspectionToleranceOperationBuilder.
NominalDMS
¶ Returns or sets the string for anglb nominal DMS
-------------------------------------
Getter Method
Signature
NominalDMS
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NominalDMS
Parameters: stringNominalDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NominalSource¶
-
InspectionToleranceOperationBuilder.
NominalSource
¶ Returns or sets the Nominal Value Source
-------------------------------------
Getter Method
Signature
NominalSource
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
NominalSource
Parameters: nominalSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProfileDispositionModeBuilder¶
-
InspectionToleranceOperationBuilder.
ProfileDispositionModeBuilder
¶ Returns the Profile Disposition Mode Builder
-------------------------------------
Getter Method
Signature
ProfileDispositionModeBuilder
Returns: Return type: NXOpen.CAM.InspectionProfileDispositionModeBuilder
New in version NX9.0.0.
License requirements: None.
SelectionFeature¶
-
InspectionToleranceOperationBuilder.
SelectionFeature
¶ Returns the selection feature
-------------------------------------
Getter Method
Signature
SelectionFeature
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionOriginFeature¶
-
InspectionToleranceOperationBuilder.
SelectionOriginFeature
¶ Returns the selection origin feature
-------------------------------------
Getter Method
Signature
SelectionOriginFeature
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionPMI¶
-
InspectionToleranceOperationBuilder.
SelectionPMI
¶ Returns the PMI selection
-------------------------------------
Getter Method
Signature
SelectionPMI
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectionTolerancedFeature¶
-
InspectionToleranceOperationBuilder.
SelectionTolerancedFeature
¶ Returns the selection toleranced feature
-------------------------------------
Getter Method
Signature
SelectionTolerancedFeature
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
StringDatumFeatName¶
-
InspectionToleranceOperationBuilder.
StringDatumFeatName
¶ Returns or sets the string datum feat name
-------------------------------------
Getter Method
Signature
StringDatumFeatName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringDatumFeatName
Parameters: stringDatumFeatName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringDatumLetter¶
-
InspectionToleranceOperationBuilder.
StringDatumLetter
¶ Returns or sets the string datum letter
-------------------------------------
Getter Method
Signature
StringDatumLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringDatumLetter
Parameters: stringDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringOriginFeatName¶
-
InspectionToleranceOperationBuilder.
StringOriginFeatName
¶ Returns or sets the string origin feat name
-------------------------------------
Getter Method
Signature
StringOriginFeatName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringOriginFeatName
Parameters: stringOriginFeatName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringPriDatum¶
-
InspectionToleranceOperationBuilder.
StringPriDatum
¶ Returns or sets the string primary datum
-------------------------------------
Getter Method
Signature
StringPriDatum
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringPriDatum
Parameters: stringPriDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringPriDatum1¶
-
InspectionToleranceOperationBuilder.
StringPriDatum1
¶ Returns or sets the string primary datum1
-------------------------------------
Getter Method
Signature
StringPriDatum1
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringPriDatum1
Parameters: stringPriDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringSecDatum¶
-
InspectionToleranceOperationBuilder.
StringSecDatum
¶ Returns or sets the string secondary datum
-------------------------------------
Getter Method
Signature
StringSecDatum
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringSecDatum
Parameters: stringSecDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringSecDatum1¶
-
InspectionToleranceOperationBuilder.
StringSecDatum1
¶ Returns or sets the string secondary datum1
-------------------------------------
Getter Method
Signature
StringSecDatum1
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringSecDatum1
Parameters: stringSecDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTerDatum¶
-
InspectionToleranceOperationBuilder.
StringTerDatum
¶ Returns or sets the string tertiary datum
-------------------------------------
Getter Method
Signature
StringTerDatum
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTerDatum
Parameters: stringTerDatum (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTerDatum1¶
-
InspectionToleranceOperationBuilder.
StringTerDatum1
¶ Returns or sets the string tertiary datum1
-------------------------------------
Getter Method
Signature
StringTerDatum1
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTerDatum1
Parameters: stringTerDatum1 (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTolName¶
-
InspectionToleranceOperationBuilder.
StringTolName
¶ Returns or sets the string tolerance name
-------------------------------------
Getter Method
Signature
StringTolName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTolName
Parameters: stringTolName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StringTolerancedFeat¶
-
InspectionToleranceOperationBuilder.
StringTolerancedFeat
¶ Returns or sets the string toleranced feat
-------------------------------------
Getter Method
Signature
StringTolerancedFeat
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringTolerancedFeat
Parameters: stringTolerancedFeat (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceProfileModeBuilder¶
-
InspectionToleranceOperationBuilder.
SurfaceProfileModeBuilder
¶ Returns the Surface Profile Mode Builder
-------------------------------------
Getter Method
Signature
SurfaceProfileModeBuilder
Returns: Return type: NXOpen.CAM.InspectionSurfaceProfileModeBuilder
New in version NX9.0.0.
License requirements: None.
TolOpType¶
-
InspectionToleranceOperationBuilder.
TolOpType
¶ Returns or sets the tolerance type
-------------------------------------
Getter Method
Signature
TolOpType
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderTolType
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolOpType
Parameters: tolOpType ( NXOpen.CAM.InspectionToleranceOperationBuilderTolType
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToleranceValueSource¶
-
InspectionToleranceOperationBuilder.
ToleranceValueSource
¶ Returns or sets the GDT Tolerance Value Source
-------------------------------------
Getter Method
Signature
ToleranceValueSource
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceValueSource
Parameters: toleranceValueSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpperDMS¶
-
InspectionToleranceOperationBuilder.
UpperDMS
¶ Returns or sets the string for anglb upper DMS
-------------------------------------
Getter Method
Signature
UpperDMS
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperDMS
Parameters: stringUpperDMS (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpperSource¶
-
InspectionToleranceOperationBuilder.
UpperSource
¶ Returns or sets the Upper Value Source
-------------------------------------
Getter Method
Signature
UpperSource
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperSource
Parameters: upperSource ( NXOpen.CAM.InspectionToleranceOperationBuilderToleranceSource
) –New in version NX9.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UseDegMin¶
-
InspectionToleranceOperationBuilder.
UseDegMin
¶ Returns or sets the deg/min flag for angle between
-------------------------------------
Getter Method
Signature
UseDegMin
Returns: Return type: NXOpen.CAM.InspectionToleranceOperationBuilderAngleFormat
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDegMin
Parameters: useDegMinSec ( NXOpen.CAM.InspectionToleranceOperationBuilderAngleFormat
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorDirection¶
-
InspectionToleranceOperationBuilder.
VectorDirection
¶ Returns or sets the vector direction
-------------------------------------
Getter Method
Signature
VectorDirection
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorDirection
Parameters: vectorDirection ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorViewVec¶
-
InspectionToleranceOperationBuilder.
VectorViewVec
¶ Returns or sets the vector view vec
-------------------------------------
Getter Method
Signature
VectorViewVec
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorViewVec
Parameters: vectorViewVec ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
XRotationDOFMode
¶ Returns or sets the x rotation dofmode
-------------------------------------
Getter Method
Signature
XRotationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationDOFMode
Parameters: xRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
XRotationLowerLimit
¶ Returns or sets the x rotation lower limit
-------------------------------------
Getter Method
Signature
XRotationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationLowerLimit
Parameters: xRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
XRotationUpperLimit
¶ Returns or sets the x rotation upper limit
-------------------------------------
Getter Method
Signature
XRotationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XRotationUpperLimit
Parameters: xRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
XTranslationDOFMode
¶ Returns or sets the x translation dofmode
-------------------------------------
Getter Method
Signature
XTranslationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationDOFMode
Parameters: xTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
XTranslationLowerLimit
¶ Returns or sets the x translation lower limit
-------------------------------------
Getter Method
Signature
XTranslationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationLowerLimit
Parameters: xTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
XTranslationUpperLimit
¶ Returns or sets the x translation upper limit
-------------------------------------
Getter Method
Signature
XTranslationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
XTranslationUpperLimit
Parameters: xTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
YRotationDOFMode
¶ Returns or sets the y rotation dofmode
-------------------------------------
Getter Method
Signature
YRotationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationDOFMode
Parameters: yRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
YRotationLowerLimit
¶ Returns or sets the y rotation lower limit
-------------------------------------
Getter Method
Signature
YRotationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationLowerLimit
Parameters: yRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
YRotationUpperLimit
¶ Returns or sets the y rotation upper limit
-------------------------------------
Getter Method
Signature
YRotationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YRotationUpperLimit
Parameters: yRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
YTranslationDOFMode
¶ Returns or sets the y translation dofmode
-------------------------------------
Getter Method
Signature
YTranslationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationDOFMode
Parameters: yTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
YTranslationLowerLimit
¶ Returns or sets the y translation lower limit
-------------------------------------
Getter Method
Signature
YTranslationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationLowerLimit
Parameters: yTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
YTranslationUpperLimit
¶ Returns or sets the y translation upper limit
-------------------------------------
Getter Method
Signature
YTranslationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
YTranslationUpperLimit
Parameters: yTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationDOFMode¶
-
InspectionToleranceOperationBuilder.
ZRotationDOFMode
¶ Returns or sets the z rotation dofmode
-------------------------------------
Getter Method
Signature
ZRotationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationDOFMode
Parameters: zRotationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationLowerLimit¶
-
InspectionToleranceOperationBuilder.
ZRotationLowerLimit
¶ Returns or sets the z rotation lower limit
-------------------------------------
Getter Method
Signature
ZRotationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationLowerLimit
Parameters: zRotationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZRotationUpperLimit¶
-
InspectionToleranceOperationBuilder.
ZRotationUpperLimit
¶ Returns or sets the z rotation upper limit
-------------------------------------
Getter Method
Signature
ZRotationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZRotationUpperLimit
Parameters: zRotationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationDOFMode¶
-
InspectionToleranceOperationBuilder.
ZTranslationDOFMode
¶ Returns or sets the z translation dofmode
-------------------------------------
Getter Method
Signature
ZTranslationDOFMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationDOFMode
Parameters: zTranslationDOFMode ( NXOpen.CAM.InspectionMethodBuilderToleranceDegreeOfFreedomMode
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationLowerLimit¶
-
InspectionToleranceOperationBuilder.
ZTranslationLowerLimit
¶ Returns or sets the z translation lower limit
-------------------------------------
Getter Method
Signature
ZTranslationLowerLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationLowerLimit
Parameters: zTranslationLowerLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZTranslationUpperLimit¶
-
InspectionToleranceOperationBuilder.
ZTranslationUpperLimit
¶ Returns or sets the z translation upper limit
-------------------------------------
Getter Method
Signature
ZTranslationUpperLimit
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZTranslationUpperLimit
Parameters: zTranslationUpperLimit (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
UpdateParameters¶
-
InspectionToleranceOperationBuilder.
UpdateParameters
¶ Updates Inspection tolerance parameters based on selected annotation.
Signature
UpdateParameters()
New in version NX7.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionToleranceOperationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.