InspectionToleranceOperationBuilderParamPriDatumModifier Enumeration¶
NXOpen.CAM.InspectionToleranceOperationBuilder.ParamPriDatumModifier is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatumModifier
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilderParamPriDatumModifier
¶ Bases:
object
Primary datum material modifiers
Enum Members
Enum Member Enum Member Description NotSet None Mmc Maximum Material Condition Lmc Least Material Condition Rfs Regardless of Feature Size -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-