InspectionSurfaceProfileModeBuilder Class¶
-
class
NXOpen.CAM.
InspectionSurfaceProfileModeBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable datum plane fitting mode enum value
New in version NX8.5.1.
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current surface profile mode |
Methods¶
Property Detail¶
Value¶
-
InspectionSurfaceProfileModeBuilder.
Value
¶ Returns or sets the current surface profile mode
-------------------------------------
Getter Method
Signature
Value
Returns: the current surface profile mode Return type: NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: itemValue ( NXOpen.CAM.InspectionMethodBuilderSurfaceProfileTypes
) – the new surface profile modeNew in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)