InspectionToleranceOperationBuilderTolType Enumeration¶
NXOpen.CAM.InspectionToleranceOperationBuilder.TolType is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderTolType
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilderTolType
¶ Bases:
object
Tolerance types
Enum Members
Enum Member Enum Member Description DistanceBetween Distance Between AngleBetween Angle Between CoordinateTolerance Coordinate Diameter Diameter Radius Radius Width Width ConeAngle Angle of Cone DatumDefinition Datum Definition Flatness Flatness Straightness Straightness Circularity Circularity Cylindricity Cylindricity LineProfile Profile of Line SurfaceProfile Profile of Surface Angularity Angularity Parallelism Parallelism Perpendicularity Perpendicularity Position Position Concentricity Concentricity Symmetry Symmetry CircularRunout Circular Runout TotalRunout Total Runout DatumTarget -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-