InspectionToleranceOperationBuilderParamPriDatum Enumeration¶
NXOpen.CAM.InspectionToleranceOperationBuilder.ParamPriDatum is an alias for NXOpen.CAM.InspectionToleranceOperationBuilderParamPriDatum
-
class
NXOpen.CAM.
InspectionToleranceOperationBuilderParamPriDatum
¶ Bases:
object
Default datum symbols
Enum Members
Enum Member Enum Member Description A A B B C C -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-