AssyFEModel Class¶
-
class
NXOpen.CAE.
AssyFEModel
¶ Bases:
NXOpen.CAE.BaseFEModel
,NXOpen.CAE.IHierarchicalFEModel
,NXOpen.CAE.IPostScenarioDataSource
This class represents an Assembly Finite Element Model. This class will act as the gateway to the Finite Element Nodes (
NXOpen.CAE.FENode
) and Elements (NXOpen.CAE.FEElement
) in the model. Only one instance of this class will exist in each assyfem part fileNew in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConnectionsContainer | Returns the universal connection container. |
ConnectionsRootFolder | Returns the root connection folder. |
FeelementLabelMap | Returns a CAE.FEElement Label to CAE.FEElement Map for this Interface to the Finite Element Model. |
FenodeLabelMap | Returns a CAE.FENode Label to CAE.FENode Map for this Interface to the Finite Element Model. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MeshManager | Returns the IMeshManager |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Parent | Returns the parent fem of this object, can be None |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AskUpdatePending | This method will inform caller if the finite element model is in an update pending state or not. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteModelEdits | Delete any Model Edits that exist on this Assembly FEM. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EnableFemUpdate | This method will enable fem update. |
Find | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAssemblyComponentForMappedFemOcc | Returns the NXOpen.Assemblies.Component in the Cad assembly fem that corresponds to an NXOpen.CAE.FEModelOccurrence . |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildren | Returns the child components of this component |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFreezeOption | Get freeze option |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMappedComponentRemovalOption | Get unmap update option |
GetMappedFemOccForAssemblyComponent | Returns the NXOpen.CAE.FEModelOccurrence in this assembly fem that corresponds to an NXOpen.Assemblies.Component . |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRepositionOption | Get reposition update option |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
MapFemToAssemblyComponent | Map a fem part to an assembly component in an assembly fem. |
MapFemToMultiAssemblyComponents | Map a fem part to multiple assembly components in an assembly fem. |
Prints a representation of this object to the system log file. | |
RemoveFemMappedToAssemblyComponent | Remove fem component mapped to assembly component in an assembly fem |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetFreezeOption | Sets freeze option |
SetMappedComponentRemovalOption | Sets unmap update option |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRepositionOption | Sets reposition update option |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UnmapFemFromAssemblyComponent | Unmap a fem part from an assembly component in an assembly fem |
UpdateFemodel | This method will update the finite element model so that it is in sync with any underlying changes. |
Enumerations¶
AssyFEModelMappedComponentRemovalType Enumeration | the unmap types |
AssyFEModelRepositionType Enumeration | the reposition types |
Property Detail¶
IsOccurrence¶
-
AssyFEModel.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
AssyFEModel.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
AssyFEModel.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
AssyFEModel.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
AssyFEModel.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Parent¶
-
AssyFEModel.
Parent
¶ Returns the parent fem of this object, can be None
-------------------------------------
Getter Method
Signature
Parent
Returns: The parent Return type: NXOpen.CAE.IFEModel
New in version NX6.0.0.
License requirements: None.
Prototype¶
-
AssyFEModel.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteModelEdits¶
-
AssyFEModel.
DeleteModelEdits
¶ Delete any Model Edits that exist on this Assembly FEM.
For example, merging coincident nodes at the assembly level may combine two nodes from different components as a single node. This method will remove these model level edits and revert the model to its original state.
Signature
DeleteModelEdits()
New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Find¶
-
AssyFEModel.
Find
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX6.0.0.
License requirements: None.
FindObject¶
-
AssyFEModel.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAssemblyComponentForMappedFemOcc¶
-
AssyFEModel.
GetAssemblyComponentForMappedFemOcc
¶ Returns the
NXOpen.Assemblies.Component
in the Cad assembly fem that corresponds to anNXOpen.CAE.FEModelOccurrence
.This relationship would have been originally established through a call to
CAE.AssyFEModel.MapFemToAssemblyComponent()
.Signature
GetAssemblyComponentForMappedFemOcc(femOcc)
Parameters: femOcc ( NXOpen.CAE.FEModelOccurrence
) – fem occurrenceReturns: component in an assembly Return type: NXOpen.Assemblies.Component
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetChildren¶
-
AssyFEModel.
GetChildren
¶ Returns the child components of this component
Signature
GetChildren()
Returns: Return type: list of NXOpen.CAE.FEModelOccurrence
New in version NX6.0.0.
License requirements: None.
GetFreezeOption¶
-
AssyFEModel.
GetFreezeOption
¶ Get freeze option
Signature
GetFreezeOption()
Returns: freeze option Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetMappedComponentRemovalOption¶
-
AssyFEModel.
GetMappedComponentRemovalOption
¶ Get unmap update option
Signature
GetMappedComponentRemovalOption()
Returns: removal option Return type: NXOpen.CAE.AssyFEModelMappedComponentRemovalType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetMappedFemOccForAssemblyComponent¶
-
AssyFEModel.
GetMappedFemOccForAssemblyComponent
¶ Returns the
NXOpen.CAE.FEModelOccurrence
in this assembly fem that corresponds to anNXOpen.Assemblies.Component
.This relationship would have been originally established through a call to
CAE.AssyFEModel.MapFemToAssemblyComponent()
.Signature
GetMappedFemOccForAssemblyComponent(cadPartOcc)
Parameters: cadPartOcc ( NXOpen.Assemblies.Component
) – component in an assemblyReturns: fem occurrence Return type: NXOpen.CAE.FEModelOccurrence
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetRepositionOption¶
-
AssyFEModel.
GetRepositionOption
¶ Get reposition update option
Signature
GetRepositionOption()
Returns: reposition option Return type: NXOpen.CAE.AssyFEModelRepositionType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MapFemToAssemblyComponent¶
-
AssyFEModel.
MapFemToAssemblyComponent
¶ Map a fem part to an assembly component in an assembly fem.
When a FEM component in an Assembly FEM is mapped to an Assembly Component in another CAD Assembly, the mapped FEM component will use the same orientation as the CAD component and will update accordingly when the orientation of the CAD component is modified.
Signature
MapFemToAssemblyComponent(femPart, cadPartOcc, workLayer)
Parameters: - femPart (
NXOpen.CAE.BaseFemPart
) – base fem part - cadPartOcc (
NXOpen.Assemblies.Component
) – component in an assembly - workLayer (bool) – true = Work layer or false = Original fem layer
Returns: fem model occurrence that represents the fem part in the assembly FEM
Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- femPart (
MapFemToMultiAssemblyComponents¶
-
AssyFEModel.
MapFemToMultiAssemblyComponents
¶ Map a fem part to multiple assembly components in an assembly fem.
When a FEM component in an Assembly FEM is mapped to an Assembly Component in another CAD Assembly, the mapped FEM component will use the same orientation as the CAD component and will update accordingly when the orientation of the CAD component is modified.
Signature
MapFemToMultiAssemblyComponents(femPart, pCadPartOccs, workLayer)
Parameters: - femPart (
NXOpen.CAE.BaseFemPart
) – base fem part - pCadPartOccs (list of
NXOpen.Assemblies.Component
) – components in cad assembly to map to - workLayer (bool) – true = Work layer or false = Original fem layer
Returns: fem model occurrences that represents the fem part in the assembly FEM
Return type: list of
NXOpen.CAE.FEModelOccurrence
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- femPart (
Print¶
-
AssyFEModel.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveFemMappedToAssemblyComponent¶
-
AssyFEModel.
RemoveFemMappedToAssemblyComponent
¶ Remove fem component mapped to assembly component in an assembly fem
Signature
RemoveFemMappedToAssemblyComponent(cadPartOcc)
Parameters: cadPartOcc ( NXOpen.Assemblies.Component
) – component in an assemblyNew in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetFreezeOption¶
-
AssyFEModel.
SetFreezeOption
¶ Sets freeze option
Signature
SetFreezeOption(freezeOption)
Parameters: freezeOption (bool) – freeze option New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetMappedComponentRemovalOption¶
-
AssyFEModel.
SetMappedComponentRemovalOption
¶ Sets unmap update option
Signature
SetMappedComponentRemovalOption(remOption)
Parameters: remOption ( NXOpen.CAE.AssyFEModelMappedComponentRemovalType
) – removal optionNew in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetName¶
-
AssyFEModel.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetRepositionOption¶
-
AssyFEModel.
SetRepositionOption
¶ Sets reposition update option
Signature
SetRepositionOption(reposOption)
Parameters: reposOption ( NXOpen.CAE.AssyFEModelRepositionType
) – reposition optionNew in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
UnmapFemFromAssemblyComponent¶
-
AssyFEModel.
UnmapFemFromAssemblyComponent
¶ Unmap a fem part from an assembly component in an assembly fem
Signature
UnmapFemFromAssemblyComponent(cadPartOcc)
Parameters: cadPartOcc ( NXOpen.Assemblies.Component
) – component in an assemblyNew in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)