AssyFEModelMappedComponentRemovalType Enumeration

NXOpen.CAE.AssyFEModel.MappedComponentRemovalType is an alias for NXOpen.CAE.AssyFEModelMappedComponentRemovalType

class NXOpen.CAE.AssyFEModelMappedComponentRemovalType

Bases: object

the unmap types

Enum Members

Enum Member Enum Member Description
KeepAsUnmapped keep unmapped
Remove remove
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.