AssyFEModelRepositionType Enumeration

NXOpen.CAE.AssyFEModel.RepositionType is an alias for NXOpen.CAE.AssyFEModelRepositionType

class NXOpen.CAE.AssyFEModelRepositionType

Bases: object

the reposition types

Enum Members

Enum Member Enum Member Description
AlwaysReposition always reposition
NeverReposition never reposition
Prompt prompt
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.