LineArrowStyleBuilder Class¶
-
class
NXOpen.Annotations.
LineArrowStyleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.LineArrowStyleBuilder
.This class queries and sets preferences that apply to leaders and arrow and extension lines when creating or editing annotations, including dimensions.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AllAroundSymbolSize | Returns or sets the size of all around symbol. |
ArrowheadIncludedAngle | Returns or sets the arrowhead included angle |
ArrowheadLength | Returns or sets the arrowhead length |
ClipOrdinateDimensionLine | Returns or sets the clipping of the dimension line to the ordinate origin at the view border |
DatumLengthPastArrow | Returns or sets the distance from the apex of the datum arrowhead to the end of the extension line |
DotArrowheadDiameter | Returns or sets the dot arrowhead diameter |
FirstArrowLineColor | Returns or sets the first arrow line color |
FirstArrowLineFont | Returns or sets the first arrow line font |
FirstArrowLineWidth | Returns or sets the first arrow line width |
FirstArrowType | Returns or sets the first arrowhead type |
FirstArrowheadColor | Returns or sets the first arrowhead color |
FirstArrowheadFont | Returns or sets the first arrowhead font |
FirstArrowheadWidth | Returns or sets the first arrowhead width |
FirstExtensionLineColor | Returns or sets the first extension line color |
FirstExtensionLineFont | Returns or sets the first extension line font |
FirstExtensionLineWidth | Returns or sets the first extension line width |
FirstJogAngle | Returns or sets the first jog angle, between the jog and the extension line, in degrees. |
FirstJogDisplay | Returns or sets the first jog’s display flag, if true, the first jog will be displayed, false otherwise |
FirstJogEndOffset | Returns or sets the first jog end offset from the dimension line |
FirstJogOrientation | Returns or sets the first jog orientation, can be either IN or OUT |
FirstJogStartOffset | Returns or sets the first jog start offset from the dimension line |
FirstPosToExtensionLineDistance | Returns or sets the distance from the position on the object being dimensioned to the end of the first extension line or arc |
LeaderLocation | Returns or sets the leader location |
LeaderOrientation | Returns or sets the leader orientation |
LinePastArrowDistance | Returns or sets the distance an extension line or arc extends past the dimension line or arc |
LinePastArrowDistance2 | Returns or sets the second distance an extension line or arc extends past the dimension line or arc |
ObliqueExtensionLineAngle | Returns or sets the extension line angle. |
SecondArrowLineColor | Returns or sets the second arrow line color |
SecondArrowLineFont | Returns or sets the second arrow line font |
SecondArrowLineWidth | Returns or sets the second arrow line width |
SecondArrowType | Returns or sets the second arrowhead type |
SecondArrowheadColor | Returns or sets the second arrowhead color |
SecondArrowheadFont | Returns or sets the second arrowhead font |
SecondArrowheadWidth | Returns or sets the second arrowhead width |
SecondExtensionLineColor | Returns or sets the second extension line color |
SecondExtensionLineFont | Returns or sets the second extension line font |
SecondExtensionLineWidth | Returns or sets the second extension line width |
SecondJogAngle | Returns or sets the second jog angle, between the jog and the extension line, in degrees. |
SecondJogDisplay | Returns or sets the second jog’s display flag, if true, the second jog will be displayed, false otherwise |
SecondJogEndOffset | Returns or sets the second jog end offset from the dimension line |
SecondJogOrientation | Returns or sets the second jog orientation, can be either IN or OUT |
SecondJogStartOffset | Returns or sets the second jog start offset from the dimension line |
SecondPosToExtensionLineDistance | Returns or sets the distance from the position on the object being dimensioned to the end of the second extension line |
StubLength | Returns or sets the stub length. |
StubSymbolType | Returns or sets the stub symbol type |
Tag | Returns the Tag for this object. |
TextOverLeaderGapFactor | Returns or sets the character size factor that controls the gap between text and the leader |
TextOverStubFactor | Returns or sets the character size factor which controls the distance between the stub and label text when the text displays above the stub line |
TextToLineDistance | Returns or sets the distance from the text to the dimension line(stub) or arc |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllAroundSymbolSize¶
-
LineArrowStyleBuilder.
AllAroundSymbolSize
¶ Returns or sets the size of all around symbol.
This is also used for inner diameter of all over symbol
-------------------------------------
Getter Method
Signature
AllAroundSymbolSize
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AllAroundSymbolSize
Parameters: allAroundSymbol (float) – New in version NX8.5.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ArrowheadIncludedAngle¶
-
LineArrowStyleBuilder.
ArrowheadIncludedAngle
¶ Returns or sets the arrowhead included angle
-------------------------------------
Getter Method
Signature
ArrowheadIncludedAngle
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadIncludedAngle
Parameters: arrowheadIncludedAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ArrowheadLength¶
-
LineArrowStyleBuilder.
ArrowheadLength
¶ Returns or sets the arrowhead length
-------------------------------------
Getter Method
Signature
ArrowheadLength
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArrowheadLength
Parameters: arrowheadLength (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ClipOrdinateDimensionLine¶
-
LineArrowStyleBuilder.
ClipOrdinateDimensionLine
¶ Returns or sets the clipping of the dimension line to the ordinate origin at the view border
-------------------------------------
Getter Method
Signature
ClipOrdinateDimensionLine
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClipOrdinateDimensionLine
Parameters: clipOrdinateDimLine (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DatumLengthPastArrow¶
-
LineArrowStyleBuilder.
DatumLengthPastArrow
¶ Returns or sets the distance from the apex of the datum arrowhead to the end of the extension line
-------------------------------------
Getter Method
Signature
DatumLengthPastArrow
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatumLengthPastArrow
Parameters: datumLengthPastArrow (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
DotArrowheadDiameter¶
-
LineArrowStyleBuilder.
DotArrowheadDiameter
¶ Returns or sets the dot arrowhead diameter
-------------------------------------
Getter Method
Signature
DotArrowheadDiameter
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DotArrowheadDiameter
Parameters: dotArrowheadDiameter (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineColor¶
-
LineArrowStyleBuilder.
FirstArrowLineColor
¶ Returns or sets the first arrow line color
-------------------------------------
Getter Method
Signature
FirstArrowLineColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineColor
Parameters: firstArrowLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineFont¶
-
LineArrowStyleBuilder.
FirstArrowLineFont
¶ Returns or sets the first arrow line font
-------------------------------------
Getter Method
Signature
FirstArrowLineFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineFont
Parameters: firstArrowLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowLineWidth¶
-
LineArrowStyleBuilder.
FirstArrowLineWidth
¶ Returns or sets the first arrow line width
-------------------------------------
Getter Method
Signature
FirstArrowLineWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowLineWidth
Parameters: firstArrowLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowType¶
-
LineArrowStyleBuilder.
FirstArrowType
¶ Returns or sets the first arrowhead type
-------------------------------------
Getter Method
Signature
FirstArrowType
Returns: Return type: NXOpen.Annotations.ArrowheadType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowType
Parameters: firstArrowType ( NXOpen.Annotations.ArrowheadType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadColor¶
-
LineArrowStyleBuilder.
FirstArrowheadColor
¶ Returns or sets the first arrowhead color
-------------------------------------
Getter Method
Signature
FirstArrowheadColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadColor
Parameters: firstArrowheadColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadFont¶
-
LineArrowStyleBuilder.
FirstArrowheadFont
¶ Returns or sets the first arrowhead font
-------------------------------------
Getter Method
Signature
FirstArrowheadFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadFont
Parameters: firstArrowheadFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstArrowheadWidth¶
-
LineArrowStyleBuilder.
FirstArrowheadWidth
¶ Returns or sets the first arrowhead width
-------------------------------------
Getter Method
Signature
FirstArrowheadWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstArrowheadWidth
Parameters: firstArrowheadWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineColor¶
-
LineArrowStyleBuilder.
FirstExtensionLineColor
¶ Returns or sets the first extension line color
-------------------------------------
Getter Method
Signature
FirstExtensionLineColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineColor
Parameters: firstExtensionLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineFont¶
-
LineArrowStyleBuilder.
FirstExtensionLineFont
¶ Returns or sets the first extension line font
-------------------------------------
Getter Method
Signature
FirstExtensionLineFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineFont
Parameters: firstExtensionLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstExtensionLineWidth¶
-
LineArrowStyleBuilder.
FirstExtensionLineWidth
¶ Returns or sets the first extension line width
-------------------------------------
Getter Method
Signature
FirstExtensionLineWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstExtensionLineWidth
Parameters: firstExtensionLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogAngle¶
-
LineArrowStyleBuilder.
FirstJogAngle
¶ Returns or sets the first jog angle, between the jog and the extension line, in degrees.
-------------------------------------
Getter Method
Signature
FirstJogAngle
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogAngle
Parameters: jogAngle (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogDisplay¶
-
LineArrowStyleBuilder.
FirstJogDisplay
¶ Returns or sets the first jog’s display flag, if true, the first jog will be displayed, false otherwise
-------------------------------------
Getter Method
Signature
FirstJogDisplay
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogDisplay
Parameters: jogDisplay (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogEndOffset¶
-
LineArrowStyleBuilder.
FirstJogEndOffset
¶ Returns or sets the first jog end offset from the dimension line
-------------------------------------
Getter Method
Signature
FirstJogEndOffset
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogEndOffset
Parameters: jogEndOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogOrientation¶
-
LineArrowStyleBuilder.
FirstJogOrientation
¶ Returns or sets the first jog orientation, can be either IN or OUT
-------------------------------------
Getter Method
Signature
FirstJogOrientation
Returns: Return type: NXOpen.Annotations.JogOrientation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogOrientation
Parameters: jogOrientation ( NXOpen.Annotations.JogOrientation
) –New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstJogStartOffset¶
-
LineArrowStyleBuilder.
FirstJogStartOffset
¶ Returns or sets the first jog start offset from the dimension line
-------------------------------------
Getter Method
Signature
FirstJogStartOffset
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstJogStartOffset
Parameters: jogStartOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
FirstPosToExtensionLineDistance¶
-
LineArrowStyleBuilder.
FirstPosToExtensionLineDistance
¶ Returns or sets the distance from the position on the object being dimensioned to the end of the first extension line or arc
-------------------------------------
Getter Method
Signature
FirstPosToExtensionLineDistance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstPosToExtensionLineDistance
Parameters: firstPosToExtensionLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LeaderLocation¶
-
LineArrowStyleBuilder.
LeaderLocation
¶ Returns or sets the leader location
-------------------------------------
Getter Method
Signature
LeaderLocation
Returns: Return type: NXOpen.Annotations.VerticalTextJustification
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderLocation
Parameters: leaderLocation ( NXOpen.Annotations.VerticalTextJustification
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LeaderOrientation¶
-
LineArrowStyleBuilder.
LeaderOrientation
¶ Returns or sets the leader orientation
-------------------------------------
Getter Method
Signature
LeaderOrientation
Returns: Return type: NXOpen.Annotations.LeaderSide
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LeaderOrientation
Parameters: leaderOrientation ( NXOpen.Annotations.LeaderSide
) –New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LinePastArrowDistance¶
-
LineArrowStyleBuilder.
LinePastArrowDistance
¶ Returns or sets the distance an extension line or arc extends past the dimension line or arc
-------------------------------------
Getter Method
Signature
LinePastArrowDistance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinePastArrowDistance
Parameters: linePastArrowDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
LinePastArrowDistance2¶
-
LineArrowStyleBuilder.
LinePastArrowDistance2
¶ Returns or sets the second distance an extension line or arc extends past the dimension line or arc
-------------------------------------
Getter Method
Signature
LinePastArrowDistance2
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinePastArrowDistance2
Parameters: linePastArrowDistance (float) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
ObliqueExtensionLineAngle¶
-
LineArrowStyleBuilder.
ObliqueExtensionLineAngle
¶ Returns or sets the extension line angle.
This angle only applies to vertical and horizontal dimensions
-------------------------------------
Getter Method
Signature
ObliqueExtensionLineAngle
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObliqueExtensionLineAngle
Parameters: obliqueExtensionLineAngle (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineColor¶
-
LineArrowStyleBuilder.
SecondArrowLineColor
¶ Returns or sets the second arrow line color
-------------------------------------
Getter Method
Signature
SecondArrowLineColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineColor
Parameters: secondArrowLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineFont¶
-
LineArrowStyleBuilder.
SecondArrowLineFont
¶ Returns or sets the second arrow line font
-------------------------------------
Getter Method
Signature
SecondArrowLineFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineFont
Parameters: secondArrowLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowLineWidth¶
-
LineArrowStyleBuilder.
SecondArrowLineWidth
¶ Returns or sets the second arrow line width
-------------------------------------
Getter Method
Signature
SecondArrowLineWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowLineWidth
Parameters: secondArrowLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowType¶
-
LineArrowStyleBuilder.
SecondArrowType
¶ Returns or sets the second arrowhead type
-------------------------------------
Getter Method
Signature
SecondArrowType
Returns: Return type: NXOpen.Annotations.ArrowheadType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowType
Parameters: secondArrowType ( NXOpen.Annotations.ArrowheadType
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadColor¶
-
LineArrowStyleBuilder.
SecondArrowheadColor
¶ Returns or sets the second arrowhead color
-------------------------------------
Getter Method
Signature
SecondArrowheadColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadColor
Parameters: secondArrowheadColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadFont¶
-
LineArrowStyleBuilder.
SecondArrowheadFont
¶ Returns or sets the second arrowhead font
-------------------------------------
Getter Method
Signature
SecondArrowheadFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadFont
Parameters: secondArrowheadFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondArrowheadWidth¶
-
LineArrowStyleBuilder.
SecondArrowheadWidth
¶ Returns or sets the second arrowhead width
-------------------------------------
Getter Method
Signature
SecondArrowheadWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondArrowheadWidth
Parameters: secondArrowheadWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineColor¶
-
LineArrowStyleBuilder.
SecondExtensionLineColor
¶ Returns or sets the second extension line color
-------------------------------------
Getter Method
Signature
SecondExtensionLineColor
Returns: Return type: Id New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineColor
Parameters: secondExtensionLineColor (Id) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineFont¶
-
LineArrowStyleBuilder.
SecondExtensionLineFont
¶ Returns or sets the second extension line font
-------------------------------------
Getter Method
Signature
SecondExtensionLineFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineFont
Parameters: secondExtensionLineFont ( NXOpen.DisplayableObjectObjectFont
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondExtensionLineWidth¶
-
LineArrowStyleBuilder.
SecondExtensionLineWidth
¶ Returns or sets the second extension line width
-------------------------------------
Getter Method
Signature
SecondExtensionLineWidth
Returns: Return type: NXOpen.Annotations.LineWidth
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondExtensionLineWidth
Parameters: secondExtensionLineWidth ( NXOpen.Annotations.LineWidth
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogAngle¶
-
LineArrowStyleBuilder.
SecondJogAngle
¶ Returns or sets the second jog angle, between the jog and the extension line, in degrees.
-------------------------------------
Getter Method
Signature
SecondJogAngle
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogAngle
Parameters: jogAngle (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogDisplay¶
-
LineArrowStyleBuilder.
SecondJogDisplay
¶ Returns or sets the second jog’s display flag, if true, the second jog will be displayed, false otherwise
-------------------------------------
Getter Method
Signature
SecondJogDisplay
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogDisplay
Parameters: jogDisplay (bool) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogEndOffset¶
-
LineArrowStyleBuilder.
SecondJogEndOffset
¶ Returns or sets the second jog end offset from the dimension line
-------------------------------------
Getter Method
Signature
SecondJogEndOffset
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogEndOffset
Parameters: jogEndOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogOrientation¶
-
LineArrowStyleBuilder.
SecondJogOrientation
¶ Returns or sets the second jog orientation, can be either IN or OUT
-------------------------------------
Getter Method
Signature
SecondJogOrientation
Returns: Return type: NXOpen.Annotations.JogOrientation
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogOrientation
Parameters: jogOrientation ( NXOpen.Annotations.JogOrientation
) –New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondJogStartOffset¶
-
LineArrowStyleBuilder.
SecondJogStartOffset
¶ Returns or sets the second jog start offset from the dimension line
-------------------------------------
Getter Method
Signature
SecondJogStartOffset
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondJogStartOffset
Parameters: jogStartOffset (float) – New in version NX10.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
SecondPosToExtensionLineDistance¶
-
LineArrowStyleBuilder.
SecondPosToExtensionLineDistance
¶ Returns or sets the distance from the position on the object being dimensioned to the end of the second extension line
-------------------------------------
Getter Method
Signature
SecondPosToExtensionLineDistance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecondPosToExtensionLineDistance
Parameters: secondPosToExtensionLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
StubLength¶
-
LineArrowStyleBuilder.
StubLength
¶ Returns or sets the stub length.
This is the size of the dogleg on a label or dimension
-------------------------------------
Getter Method
Signature
StubLength
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubLength
Parameters: stubLength (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
StubSymbolType¶
-
LineArrowStyleBuilder.
StubSymbolType
¶ Returns or sets the stub symbol type
-------------------------------------
Getter Method
Signature
StubSymbolType
Returns: Return type: NXOpen.Annotations.StubSymbolType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StubSymbolType
Parameters: stubSymbolType ( NXOpen.Annotations.StubSymbolType
) –New in version NX11.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextOverLeaderGapFactor¶
-
LineArrowStyleBuilder.
TextOverLeaderGapFactor
¶ Returns or sets the character size factor that controls the gap between text and the leader
-------------------------------------
Getter Method
Signature
TextOverLeaderGapFactor
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextOverLeaderGapFactor
Parameters: textOverLeaderGapFactor (float) – New in version NX8.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextOverStubFactor¶
-
LineArrowStyleBuilder.
TextOverStubFactor
¶ Returns or sets the character size factor which controls the distance between the stub and label text when the text displays above the stub line
-------------------------------------
Getter Method
Signature
TextOverStubFactor
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextOverStubFactor
Parameters: textOverStubFactor (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
TextToLineDistance¶
-
LineArrowStyleBuilder.
TextToLineDistance
¶ Returns or sets the distance from the text to the dimension line(stub) or arc
-------------------------------------
Getter Method
Signature
TextToLineDistance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TextToLineDistance
Parameters: textToLineDistance (float) – New in version NX6.0.0.
License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
LineArrowStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.