VerticalTextJustification Enumeration

class NXOpen.Annotations.VerticalTextJustification

Bases: object

Represents the vertical text justification Enum Members

Enum Member Enum Member Description
Top
Middle
Bottom
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.