LineWidth Enumeration¶
-
class
NXOpen.Annotations.
LineWidth
¶ Bases:
object
Specifies the line width. When using a standard font in the
NXOpen.Annotations.LetteringStyleBuilder
the values forNXOpen.Annotations.LineWidth
will be interpreted as follows: A value ofNXOpen.Annotations.LineWidth.Thin
is equivalent to a font style value of “Regular” or “Italic” (if italic is set). Any value other thanNXOpen.Annotations.LineWidth.Thin
is equivalent to a font style value of “Bold” or “Bold Italic” (if italic is set). This applies to:NXOpen.Annotations.LetteringStyleBuilder.DimensionTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.DimensionTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.AppendedTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.AppendedTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.ToleranceTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.ToleranceTextItalicized`()
NXOpen.Annotations.LetteringStyleBuilder.GeneralTextLineWidth`()
with respect toNXOpen.Annotations.LetteringStyleBuilder.GeneralTextItalicized`()
Enum MembersEnum Member Enum Member Description Normal Thick Thin One Width One Two Width Two Three Width Three Four Width Four Five Width Five Six Width Six Seven Width Seven Eight Width Eight Nine Width Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-