LeaderSide Enumeration¶
-
class
NXOpen.Annotations.
LeaderSide
¶ Bases:
object
Specifies which side the leader will be on Enum Members
Enum Member Enum Member Description Null Should not be used Left Right Inferred When used with NXOpen API, leader side will be set to Left by default. This is only used while interacting with NX UI Last Last enum value. Should not be used. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-