DisplayableObjectObjectFont Enumeration¶
NXOpen.DisplayableObject.ObjectFont is an alias for NXOpen.DisplayableObjectObjectFont
-
class
NXOpen.
DisplayableObjectObjectFont
¶ Bases:
object
specifies the object font for objects such as lines
New in version NX3.0.0.
Enum Members
Enum Member Enum Member Description Solid Dashed Phantom Centerline Dotted LongDashed DottedDashed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-