Interface | Description |
---|---|
AlignShellElementNormalBuilder |
Represents a
AlignShellElementNormalBuilder builder used to align the normals of
connected shell elements with a seed shell element. |
DuplicateElementsCheckBuilder |
Represents a
DuplicateElementsCheckBuilder
to check for duplicate elements within the candidate elements. |
DuplicateNodesCheckBuilder |
Represents a
DuplicateNodesCheckBuilder
to check for duplicate nodes within the candidate nodes. |
ElementEdgeCheckBuilder |
Represents a
ElementEdgeCheckBuilder which can be
used to detect free element edges or non-manifold edges. |
ElementMaterialOrientationCheckBuilder |
Represents a
ElementMaterialOrientationCheckBuilder
used to check the material orientation for shell and solid elements. |
ElementQualityCheckBuilder |
Represents a
ElementQualityCheckBuilder to
perform quality checking on the candidate elements. |
ElementQualityCheckResults |
Represents the element quality checking result of
ElementQualityCheckBuilder
To obtain an instance of this class use CAE.ModelCheck.ElementQualityCheckBuilder Created in NX8.5.0 |
ElementQualitySetting |
Represents element quality check settings of a specified solver language.
|
ElementQualitySettingCollection |
Represents a collection of
ElementQualitySetting in a cae part. |
ElementSpecificTestValue |
Represents the quality setting for a specfied element reference
Not to support KF . |
ElementTestResult |
Represents quality checking result for an element.
|
FaceClearanceCheckBuilder |
Represents a
FaceClearanceCheckBuilder to perform polygon face
interference or clearance check. |
ITestValue |
Represents the quality check criteria value settings
This is an abstract class, and cannot be instantiated. |
ModelSetupCheckBuilder |
Represents a
ModelSetupCheckBuilder which can be
used to check if the active SimSolution contains all the necessary
items for the analysis, including elements, loads, constraints and materials. |
QualityTestValue |
Represents quality test settings of a specified test type
Not to support KF . |
ReverseShellElementNormalBuilder |
Represents a
ReverseShellElementNormalBuilder used to reverse normals
for specified shell elements. |
SolidElementFaceNormalBuilder |
Represents a
SolidElementFaceNormalBuilder used to reorient normals
for left handed solid elements. |
TestResult |
Represents quality checking result of a quality test
To obtain an instance of this class use CAE.ModelCheck.ElementTestResult.GetTestResults Created in NX8.5.0 |
TestValueTypes |
Represents the quality check criteria value settings
No Creator this holds an enum shared by other classes . |
Class | Description |
---|---|
AlignShellElementNormalBuilder.ConnectedElementScope |
the options to define the connection scope to the seed element for model checking
|
DuplicateElementsCheckBuilder.DeletePreference |
Represents the duplicate elements deleting preference
|
DuplicateElementsCheckBuilder.DisplaySettings |
Represents the display settings of duplicated elements detected
|
DuplicateNodesCheckBuilder.DisplaySettings |
Represents the display settings data
|
DuplicateNodesCheckBuilder.ListOption |
Represents the duplicate nodes merging preference
|
DuplicateNodesCheckBuilder.MergePreference |
Represents the duplicate nodes merging preference
|
ElementEdgeCheckBuilder.DoCheckData |
This class holds the data returned from
ElementEdgeCheckBuilder.doCheck() |
ElementEdgeCheckBuilder.EdgeDisplayStyle |
the display style of the edges detected
|
ElementEdgeCheckBuilder.ExecuteCheckData |
This class holds the data returned from
ElementEdgeCheckBuilder.executeCheck() |
ElementEdgeCheckBuilder.Scope |
the Scope over which the Computation of free/non-manifold edges with be done
|
ElementMaterialOrientationCheckBuilder.DoCheckData |
This class holds the data returned from
ElementMaterialOrientationCheckBuilder.doCheck() |
ElementMaterialOrientationCheckBuilder.MaterialOrientationType |
the material orientation type
|
ElementQualityCheckBuilder.OutputElements |
indicates how to create output group
|
ElementQualityCheckBuilder.ReportFormat |
indicates how to generate report
|
ElementQualityCheckResults.TestSummary |
Reprents the summary data of a specified quality checking test type
|
ElementQualitySetting.LimitValue |
indicates how criteria value is defined
|
ITestValue.CriteriaValueData |
This class holds the data returned from
ITestValue.getCriteriaValue(nxopen.cae.modelcheck.TestValueTypes.CriteriaType) |
ITestValue.IsSolverSpecificTestData |
This class holds the data returned from
ITestValue.getIsSolverSpecificTest() |
ReverseShellElementNormalBuilder.DisplayTypeValue |
indicates how display type value is defined
|
TestValueTypes.CriteriaType |
the alert level of a criteria value
|
TestValueTypes.ElementReference |
represents an element reference definition associated with this test
|
TestValueTypes.Result |
the checking result
|
TestValueTypes.TestType |
the test types
|
TestValueTypes.Validator |
indicates how to compare the check result with the criteria value
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.