public static class TestValueTypes.CriteriaType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ERROR
reports as error if the check result failed with the criteria value
|
static int |
_WARNING
reports as warning if the check result failed with the criteria value
|
static TestValueTypes.CriteriaType |
ERROR
reports as error if the check result failed with the criteria value
|
static TestValueTypes.CriteriaType |
WARNING
reports as warning if the check result failed with the criteria value
|
Modifier and Type | Method and Description |
---|---|
static TestValueTypes.CriteriaType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TestValueTypes.CriteriaType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TestValueTypes.CriteriaType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TestValueTypes.CriteriaType WARNING
public static final TestValueTypes.CriteriaType ERROR
public static final int _WARNING
public static final int _ERROR
public static TestValueTypes.CriteriaType valueOf(int value)
public static TestValueTypes.CriteriaType valueOf(String name)
public static TestValueTypes.CriteriaType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.