public interface SimSolution extends SimGroupContainer, IReportCollection
SimSimulation.createSolution(java.lang.String, java.lang.String, java.lang.String, java.lang.String)
Modifier and Type | Interface and Description |
---|---|
static class |
SimSolution.ConflictingBcPairByIndexData
This class holds the data returned from
getConflictingBcPairByIndex(int) |
static class |
SimSolution.ConflictingConstraintPairByIndexData
This class holds the data returned from
getConflictingConstraintPairByIndex(int) |
static class |
SimSolution.ResultFileData
This class holds the data returned from
getResultFile() |
static class |
SimSolution.SetupCheckOption
Model Setup Check Options
|
static class |
SimSolution.SolveMode
Run Mode Options
|
static class |
SimSolution.SolveOption
Solve Options
|
static class |
SimSolution.StepPosition
Step creation options
|
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
SimSimulation.AxisymAbstractionType |
abstractionType()
Returns the abstraction type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolutionStep |
activeStep()
Returns the active step
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
addBc(SimBC bc)
Add the bc to the solution
Only the BC that not under the folder can be added to solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
addFolder(SimLbcFolder folder)
Add the folder to the solution
Only the folder not under other folder can be added to solution.
|
void |
addPrerequisite(SimSolution prerequisite)
Adds a prerequisite to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
addStep(SimSolutionStep step)
Adds a step to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
allowedStepTypeCount()
Returns the count of allowable step types
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
String |
analysisType()
Returns the analysis type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
applySolverLanguageExportOptions(CaeDataContainer propertyList)
Stores the solver language export options to the specified solution.
|
int |
conflictingBcCount()
Returns the number of conflicting BC pairs in this solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
conflictingConstraintsCount()
Deprecated.
Deprecated in NX10.0.0. Use
conflictingBcCount() instead.
|
CorrelAlignmentBuilder |
createAlignmentBuilder()
Creates the builder object for test and imported solution alignment dialog
License requirements: nx_correl_base ("FE Correlation") . |
ConflictResolutionBuilder |
createConflictResolutionBuilder(SimGroupContainer tStep,
SimBC tBc1,
SimBC tBc2)
Creates a conflict resolution builder for this input pair of BCs
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
ConstraintResolutionBuilder |
createConstraintResolutionBuilder(SimGroupContainer tStep,
SimConstraint tConstraint1,
SimConstraint tConstraint2)
Deprecated.
Deprecated in NX10.0.0. Use
createConflictResolutionBuilder(nxopen.cae.SimGroupContainer, nxopen.cae.SimBC, nxopen.cae.SimBC) instead.
|
ResultProbeBuilder |
createResultProbeBuilder(ResultProbe resultProbe)
Creates the builder to create and edit Result Probe object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolutionStep |
createStep(int stepType,
boolean makeActive,
String stepName)
Creates a step, adds it to the solution and optionally makes it the Active Step.
|
SimSolutionStep |
createStep(int stepType,
boolean makeActive,
String stepName,
SimSolution.StepPosition position,
SimSolutionStep relativeStep)
Create a step at the specified position, add to the solution and optionally make it active
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolutionStep |
createStep(int stepType,
String stepName)
Creates a step and add to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
deleteStep(SimSolutionStep step)
Removes a step from the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
TaggedObject |
find(String journalIdentifier)
Returns the children of the Solution of the given Identifier
License requirements: None. |
ResultProbe[] |
getAllResultProbes()
Get all result probe in solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimBC[] |
getBcs()
Gets all the BCs in this solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution.ConflictingBcPairByIndexData |
getConflictingBcPairByIndex(int index)
Returns the nth conflicting BC pair, where the index is between 0 and
conflictingBcCount() - 1
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX10.0.0 |
SimSolution.ConflictingConstraintPairByIndexData |
getConflictingConstraintPairByIndex(int index)
Deprecated.
Deprecated in NX10.0.0. Use
getConflictingBcPairByIndex(int) instead.
|
String |
getDisplayNameOfSolutionType()
Get the display name of solution type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
String |
getDisplayNameOfSolverType()
Get the display name of solver type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimLbcFolder[] |
getFolders()
Gets all the root folders in this solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
String |
getManagedResultFile()
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :getManagedResultFile() instead.
|
SimSolution.ResultFileData |
getResultFile()
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :getResultFile() instead.
|
Unit[] |
getResultFileUnits()
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :getResultFileUnits() instead.
|
SimResultReference |
getResultReferenceByIndex(int resultIndex)
Returns the Result Reference at the index passed
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolutionStep |
getStepByIndex(int stepIndex)
Returns the step at the index passed
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimBC[] |
getUnfolderedBcs()
Gets all the unfoldered BCs in this solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
moveStep(SimSolutionStep stepToMove,
SimSolution.StepPosition position,
SimSolutionStep relativeStep)
Moves step to the specified position
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
PropertyTable |
propertyTable()
Returns the property table associated with the solution object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
removeAllConstraints()
Remove all constraints from the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
removeAllLoads()
Remove all loads from the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
removeAllSimulationObjects()
Remove all simulation objects from the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
removeBc(SimBC bc)
Remove the bc from the solution
Only the BC that not under the folder can be remove from solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
removeFolder(SimLbcFolder folder)
Remove the folder from the solution
Only the folder not under other folder can be removed from solution.
|
void |
removePrerequisite(SimSolution prerequisite)
Remove a prerequisite to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
rename(String name,
boolean renameResults)
Rename Solution and optionally rename associated results files
License requirements: None. |
void |
resolveConstraintConflicts()
Runs the Assisted Conflict Check Mechanism for all constraints
SimConstraint
in an active solution SimSolution and/or in an active step SimSolutionStep ,
generating new constraints SimConstraint if there is any conflcit between the constraints. |
int |
resultReferenceCount()
Returns the number of Result References
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setActiveStep(SimSolutionStep activeStep)
Sets the active step
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setFemValidInPost(boolean valid)
Specify whether NX Post should group entities based on
node and element groups and meshes in the pre-processing model
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setInferredResultFile()
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :setInferredResultFile() instead.
|
void |
setInferredResultFileUnits()
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :setInferredResultFileUnits() instead.
|
void |
setLocalResultFile(String dirpath,
String filename)
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :setLocalResultFile(java.lang.String, java.lang.String) instead.
|
void |
setManagedResultFile(String file)
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :setManagedResultFile(java.lang.String) instead.
|
void |
setResultFileUnits(Unit[] units)
Deprecated.
Deprecated in NX10.0.0. Use
SimResultReference :setResultFileUnits(nxopen.Unit[]) instead.
|
void |
setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce)
Set the time properties for this solution based on the given condition sequences
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce,
double stepSize,
Unit stepUnit)
Set the time properties for this solution based on the given condition sequences and integration step size
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce,
int numSteps)
Set the time properties for this solution based on the given condition sequences and number of integration steps
License requirements: nx_masterfem ("Finite Element Modeling") . |
String |
solutionType()
Returns the solution type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
solve(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption)
Solves the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
PropertyTable |
solverOptionsPropertyTable()
Returns the property table associated with the solution's solver options
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
String |
solverType()
Returns the solver type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
stepCount()
Returns the number of steps
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
updateFromLoadRecipe()
Update steps and loads of this solution created from load recipe
License requirements: None. |
createConstraintGroup, createLoadGroup, createSimulationObjectGroup, deleteGroup, getGroupCount, getGroups, isConstraintGroupAllowed, isLoadGroupAllowed, isSimulationObjectGroupAllowed
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
createReport, getReports
void rename(String name, boolean renameResults) throws NXException, RemoteException
name
- new solution namerenameResults
- true if you what associated results files to be renamed as wellNXException
RemoteException
PropertyTable propertyTable() throws NXException, RemoteException
NXException
RemoteException
PropertyTable solverOptionsPropertyTable() throws NXException, RemoteException
NXException
RemoteException
void addStep(SimSolutionStep step) throws NXException, RemoteException
step
- solution step to be addedNXException
RemoteException
SimSolutionStep createStep(int stepType, String stepName) throws NXException, RemoteException
stepType
- index of the step typestepName
- name of the stepSimSolutionStep
to be addedNXException
RemoteException
SimSolutionStep createStep(int stepType, boolean makeActive, String stepName) throws NXException, RemoteException
stepType
- index of the step typemakeActive
- if true the step will be made the active stepstepName
- name of the stepSimSolutionStep
to be addedNXException
RemoteException
SimSolutionStep createStep(int stepType, boolean makeActive, String stepName, SimSolution.StepPosition position, SimSolutionStep relativeStep) throws NXException, RemoteException
stepType
- index of the step typemakeActive
- if true the step will be made the active stepstepName
- name of the stepposition
- relative positionrelativeStep
- the step with respect to which the relative position is specifiedSimSolutionStep
to be addedNXException
RemoteException
void moveStep(SimSolutionStep stepToMove, SimSolution.StepPosition position, SimSolutionStep relativeStep) throws NXException, RemoteException
stepToMove
- step to moveposition
- relative positionrelativeStep
- the step with respect to which the relative position is specifiedNXException
RemoteException
int allowedStepTypeCount() throws NXException, RemoteException
NXException
RemoteException
void deleteStep(SimSolutionStep step) throws NXException, RemoteException
step
- step SimSolutionStep
to be addedNXException
RemoteException
SimSolutionStep activeStep() throws NXException, RemoteException
SimSolutionStep
NXException
RemoteException
void setActiveStep(SimSolutionStep activeStep) throws NXException, RemoteException
activeStep
- active step SimSolutionStep
NXException
RemoteException
int stepCount() throws NXException, RemoteException
SimSolutionStep
NXException
RemoteException
SimSolutionStep getStepByIndex(int stepIndex) throws NXException, RemoteException
stepIndex
- index of the stepSimSolutionStep
at the indexNXException
RemoteException
void addPrerequisite(SimSolution prerequisite) throws NXException, RemoteException
prerequisite
- prerequisite solution to be addedNXException
RemoteException
void removePrerequisite(SimSolution prerequisite) throws NXException, RemoteException
prerequisite
- prerequisite solution to be removedNXException
RemoteException
String solverType() throws NXException, RemoteException
NXException
RemoteException
String getDisplayNameOfSolverType() throws NXException, RemoteException
NXException
RemoteException
String analysisType() throws NXException, RemoteException
NXException
RemoteException
String solutionType() throws NXException, RemoteException
NXException
RemoteException
String getDisplayNameOfSolutionType() throws NXException, RemoteException
NXException
RemoteException
SimSimulation.AxisymAbstractionType abstractionType() throws NXException, RemoteException
NXException
RemoteException
void addBc(SimBC bc) throws NXException, RemoteException
bc
- the bc to be addedNXException
RemoteException
void removeBc(SimBC bc) throws NXException, RemoteException
bc
- the bc to be removedNXException
RemoteException
void removeAllConstraints() throws NXException, RemoteException
NXException
RemoteException
void removeAllLoads() throws NXException, RemoteException
NXException
RemoteException
void removeAllSimulationObjects() throws NXException, RemoteException
NXException
RemoteException
void addFolder(SimLbcFolder folder) throws NXException, RemoteException
folder
- the folder to be addedNXException
RemoteException
void removeFolder(SimLbcFolder folder) throws NXException, RemoteException
folder
- the folder to be removedNXException
RemoteException
SimBC[] getBcs() throws NXException, RemoteException
NXException
RemoteException
SimLbcFolder[] getFolders() throws NXException, RemoteException
NXException
RemoteException
SimBC[] getUnfolderedBcs() throws NXException, RemoteException
NXException
RemoteException
void resolveConstraintConflicts() throws NXException, RemoteException
SimConstraint
in an active solution SimSolution
and/or in an active step SimSolutionStep
,
generating new constraints SimConstraint
if there is any conflcit between the constraints.
NXException
RemoteException
void solve(SimSolution.SolveOption solveOption, SimSolution.SetupCheckOption setupCheckOption) throws NXException, RemoteException
solveOption
- solve optionsetupCheckOption
- setup check optionNXException
RemoteException
CorrelAlignmentBuilder createAlignmentBuilder() throws NXException, RemoteException
NXException
RemoteException
int conflictingConstraintsCount() throws NXException, RemoteException
conflictingBcCount()
instead.
SimConstraint
NXException
RemoteException
int conflictingBcCount() throws NXException, RemoteException
SimBC
NXException
RemoteException
SimSolution.ConflictingConstraintPairByIndexData getConflictingConstraintPairByIndex(int index) throws NXException, RemoteException
getConflictingBcPairByIndex(int)
instead.
conflictingConstraintsCount()
- 1
index
- index of the conflicting constraint pair, which is between 0 and conflictingConstraintsCount()
- 1
NXException
RemoteException
SimSolution.ConflictingBcPairByIndexData getConflictingBcPairByIndex(int index) throws NXException, RemoteException
conflictingBcCount()
- 1
index
- index of the conflicting BC pair, which is between 0 and conflictingBcCount()
- 1NXException
RemoteException
ConstraintResolutionBuilder createConstraintResolutionBuilder(SimGroupContainer tStep, SimConstraint tConstraint1, SimConstraint tConstraint2) throws NXException, RemoteException
createConflictResolutionBuilder(nxopen.cae.SimGroupContainer, nxopen.cae.SimBC, nxopen.cae.SimBC)
instead.
tStep
- solution step. can be same as solutiontConstraint1
- first constraint in conflicttConstraint2
- second constraint in conflict
NXException
RemoteException
ConflictResolutionBuilder createConflictResolutionBuilder(SimGroupContainer tStep, SimBC tBc1, SimBC tBc2) throws NXException, RemoteException
tStep
- solution step. can be same as solutiontBc1
- first BC in conflicttBc2
- second BC in conflictNXException
RemoteException
void applySolverLanguageExportOptions(CaeDataContainer propertyList) throws NXException, RemoteException
propertyList
- the export option parameters. See CAE.CaeSession#getDataContainer
.NXException
RemoteException
void setFemValidInPost(boolean valid) throws NXException, RemoteException
valid
- valid or notNXException
RemoteException
void setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce) throws NXException, RemoteException
conditionSeqeunce
- populate solution time properties from SimConditionSequence
NXException
RemoteException
void setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce, int numSteps) throws NXException, RemoteException
conditionSeqeunce
- populate solution time properties from SimConditionSequence
numSteps
- number of integration stepsNXException
RemoteException
void setTimePropsFromConditionSequence(SimConditionSequence conditionSeqeunce, double stepSize, Unit stepUnit) throws NXException, RemoteException
conditionSeqeunce
- populate solution time properties from SimConditionSequence
stepSize
- size of integration stepsstepUnit
- step size Unit
NXException
RemoteException
ResultProbeBuilder createResultProbeBuilder(ResultProbe resultProbe) throws NXException, RemoteException
resultProbe
- NXException
RemoteException
int resultReferenceCount() throws NXException, RemoteException
SimResultReference
NXException
RemoteException
SimResultReference getResultReferenceByIndex(int resultIndex) throws NXException, RemoteException
resultIndex
- index of the result referenceSimResultReference
at the indexNXException
RemoteException
void setLocalResultFile(String dirpath, String filename) throws NXException, RemoteException
SimResultReference
:setLocalResultFile(java.lang.String, java.lang.String)
instead.
dirpath
- directory namefilename
- file name
NXException
RemoteException
void setManagedResultFile(String file) throws NXException, RemoteException
SimResultReference
:setManagedResultFile(java.lang.String)
instead.
file
- file name
NXException
RemoteException
void setInferredResultFile() throws NXException, RemoteException
SimResultReference
:setInferredResultFile()
instead.
NXException
RemoteException
SimSolution.ResultFileData getResultFile() throws NXException, RemoteException
SimResultReference
:getResultFile()
instead.
NXException
RemoteException
String getManagedResultFile() throws NXException, RemoteException
SimResultReference
:getManagedResultFile()
instead.
NXException
RemoteException
Unit[] getResultFileUnits() throws NXException, RemoteException
SimResultReference
:getResultFileUnits()
instead.
NXException
RemoteException
void setResultFileUnits(Unit[] units) throws NXException, RemoteException
SimResultReference
:setResultFileUnits(nxopen.Unit[])
instead.
units
- 6 units for mass, length, time, temperature, angle, and thermal energy
NXException
RemoteException
void setInferredResultFileUnits() throws NXException, RemoteException
SimResultReference
:setInferredResultFileUnits()
instead.
NXException
RemoteException
void updateFromLoadRecipe() throws NXException, RemoteException
NXException
RemoteException
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
journalIdentifier
- Journal identifier of the objectNXException
RemoteException
ResultProbe[] getAllResultProbes() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.