public interface ConflictResolutionBuilder extends Builder
ConflictResolutionBuilder
builder which can resolve conflicts between the two input BCs by a specified rule SimSolution.createConflictResolutionBuilder(nxopen.cae.SimGroupContainer, nxopen.cae.SimBC, nxopen.cae.SimBC)
Modifier and Type | Interface and Description |
---|---|
static class |
ConflictResolutionBuilder.Rule
Conflict Resolution Rule
|
Modifier and Type | Method and Description |
---|---|
PropertyTable |
propertyTable()
Returns the new BC's property table which can be used to update its property
License requirements: None. |
ConflictResolutionBuilder.Rule |
resolveRule()
Returns the resolution rule which will be used to resolve the conflict between the two input BCs
License requirements: None. |
void |
setResolveRule(ConflictResolutionBuilder.Rule resolutionRule)
License requirements: nx_masterfem ("Finite Element Modeling") . |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
PropertyTable propertyTable() throws NXException, RemoteException
NXException
RemoteException
ConflictResolutionBuilder.Rule resolveRule() throws NXException, RemoteException
NXException
RemoteException
void setResolveRule(ConflictResolutionBuilder.Rule resolutionRule) throws NXException, RemoteException
resolutionRule
- NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.