public static class AlignShellElementNormalBuilder.ConnectedElementScope extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL_VISIBLE
Limits check to only those shell elements which are connected to the Seed Element and are currently visible
|
static int |
_SEED_MESH
Limits check to only those shell elements in the mesh that contains the Seed Element
|
static int |
_USER_SPECIFIED
Limits check to only those shell elements specified in
AlignShellElementNormalBuilder.userSpecifiedConnectElements() |
static AlignShellElementNormalBuilder.ConnectedElementScope |
ALL_VISIBLE
Limits check to only those shell elements which are connected to the Seed Element and are currently visible
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
SEED_MESH
Limits check to only those shell elements in the mesh that contains the Seed Element
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
USER_SPECIFIED
Limits check to only those shell elements specified in
AlignShellElementNormalBuilder.userSpecifiedConnectElements() |
Modifier and Type | Method and Description |
---|---|
static AlignShellElementNormalBuilder.ConnectedElementScope |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlignShellElementNormalBuilder.ConnectedElementScope |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlignShellElementNormalBuilder.ConnectedElementScope[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlignShellElementNormalBuilder.ConnectedElementScope SEED_MESH
public static final AlignShellElementNormalBuilder.ConnectedElementScope ALL_VISIBLE
public static final AlignShellElementNormalBuilder.ConnectedElementScope USER_SPECIFIED
AlignShellElementNormalBuilder.userSpecifiedConnectElements()
public static final int _SEED_MESH
public static final int _ALL_VISIBLE
public static final int _USER_SPECIFIED
AlignShellElementNormalBuilder.userSpecifiedConnectElements()
public static AlignShellElementNormalBuilder.ConnectedElementScope valueOf(int value)
public static AlignShellElementNormalBuilder.ConnectedElementScope valueOf(String name)
public static AlignShellElementNormalBuilder.ConnectedElementScope[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.