See: Description
Interface | Description |
---|---|
CoordinatesLocation |
Location interface.
|
Element |
This is the class to access a connection element
To obtain an instance of this object use the Create creator in CAE.Connections.ElementCollection . |
ElementCollection |
Element collection provides methods to manage
CAE.Connections.Element objects
To obtain an instance of this class, refer to BaseFEModel Created in NX11.0.0 |
Folder |
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder. |
IConnection |
This class represents an interface to a connection object.
|
IConnectionMod |
This class represents an interface to a connection object.
|
IDiameterDefinition |
This class represents an Interface to the Diameter parameters.
|
IFlangeContainer |
This interface offers access to the flanges of a connection (SpotWeld for example).
|
IHeightDefinition |
This class represents an Interface to the Height parameters.
|
ILocationContainer |
This class represents an Interface to the Locations parameters.
|
ITolerance |
This class represents an Interface to the Tolerance parameters.
|
Location |
Location base class.
|
NodeLocation |
Location interface.
|
PointLocation |
Location interface.
|
SpotWeld |
Spot Weld connection.
|
Class | Description |
---|---|
ConnectionType |
Connection type
|
DiameterType |
Diameter definition types
|
ElementStatusType |
Element status
|
ElementType |
Element type
|
HeightType |
Types of height definitions
|
LocationType |
Location type
|
MaterialType |
Material definition types
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.