public class DiameterType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FORMULA
Formula defined diameter
|
static int |
_USER
User defined diameter
|
static DiameterType |
FORMULA
Formula defined diameter
|
static DiameterType |
USER
User defined diameter
|
Modifier and Type | Method and Description |
---|---|
static DiameterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DiameterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DiameterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DiameterType USER
public static final DiameterType FORMULA
public static final int _USER
public static final int _FORMULA
public static DiameterType valueOf(int value)
public static DiameterType valueOf(String name)
public static DiameterType[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.