public interface Folder extends NXObject
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
void |
addFolder(Folder subfolder)
Add a subfolder to this folder.
|
Folder |
createFolder(String name)
Creates a
CAE.Connections.Folder in this folder with the specified name
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX11.0.0 |
SpotWeld |
createSpotWeld(String name)
Create a
CAE.Connections.SpotWeld in this folder with the specified name
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX11.0.0 |
IConnection[] |
importConnectionsFromMcf(String file,
Unit inputFileUnit)
Create
CAE.Connections.IConnection connections in the current CAE.Connections.Folder
using connection data imported from a MCF file. |
SpotWeld[] |
importSpotWeldWcd(String file,
Unit inputFileUnit)
Create
CAE.Connections.SpotWeld connections in the current CAE.Connections.Folder
using connection data imported from a WCD file. |
void |
moveConnectionToThisFolder(IConnectionMod connection)
Add a connection to this folder.
|
String |
name()
Returns the name of the connection folder.
|
void |
setName(String name)
License requirements: nx_masterfem ("Finite Element Modeling") . |
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, owningComponent, owningPart, print, prototype
Folder createFolder(String name) throws NXException, RemoteException
CAE.Connections.Folder
in this folder with the specified name
name
- Name that the created folder should haveCAE.Connections.Folder
NXException
RemoteException
SpotWeld createSpotWeld(String name) throws NXException, RemoteException
CAE.Connections.SpotWeld
in this folder with the specified name
name
- name of the connectionNXException
RemoteException
String name() throws NXException, RemoteException
name
in interface INXObject
NXException
RemoteException
void setName(String name) throws NXException, RemoteException
setName
in interface INXObject
name
- NXException
RemoteException
void addFolder(Folder subfolder) throws NXException, RemoteException
subfolder
- NXException
RemoteException
void moveConnectionToThisFolder(IConnectionMod connection) throws NXException, RemoteException
connection
- NXException
RemoteException
SpotWeld[] importSpotWeldWcd(String file, Unit inputFileUnit) throws NXException, RemoteException
CAE.Connections.SpotWeld
connections in the current CAE.Connections.Folder
using connection data imported from a WCD file.
file
- name of the import fileinputFileUnit
- the length unit used in the input fileNXException
RemoteException
IConnection[] importConnectionsFromMcf(String file, Unit inputFileUnit) throws NXException, RemoteException
CAE.Connections.IConnection
connections in the current CAE.Connections.Folder
using connection data imported from a MCF file.
file
- name of the import fileinputFileUnit
- the length unit used in the input fileNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.