Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Class and Description |
---|
ElementCollection
Element collection provides methods to manage
CAE.Connections.Element objects
To obtain an instance of this class, refer to BaseFEModel Created in NX11.0.0 |
Folder
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder. |
Class and Description |
---|
ConnectionType
Connection type
|
CoordinatesLocation
Location interface.
|
DiameterType
Diameter definition types
|
Element
This is the class to access a connection element
To obtain an instance of this object use the Create creator in CAE.Connections.ElementCollection . |
ElementStatusType
Element status
|
ElementType
Element type
|
Folder
The Folder class offers a way to create a hierarchy of connections and sub-folders
To obtain an instance of this object use the add_folder creator in a parent folder. |
HeightType
Types of height definitions
|
IConnection
This class represents an interface to a connection object.
|
IConnectionMod
This class represents an interface to a connection object.
|
IDiameterDefinition
This class represents an Interface to the Diameter parameters.
|
IFlangeContainer
This interface offers access to the flanges of a connection (SpotWeld for example).
|
IHeightDefinition
This class represents an Interface to the Height parameters.
|
ILocationContainer
This class represents an Interface to the Locations parameters.
|
ITolerance
This class represents an Interface to the Tolerance parameters.
|
Location
Location base class.
|
LocationType
Location type
|
MaterialType
Material definition types
|
NodeLocation
Location interface.
|
PointLocation
Location interface.
|
SpotWeld
Spot Weld connection.
|
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.