public interface IFEModel extends NXObject
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
FEElementLabelMap |
feelementLabelMap()
Returns a
CAE.FEElement Label to CAE.FEElement Map
for this Interface to the Finite Element Model. |
FENodeLabelMap |
fenodeLabelMap()
Returns a
CAE.FENode Label to CAE.FENode Map for this
Interface to the Finite Element Model. |
IMeshManager |
meshManager()
Returns the IMeshManager
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
IMeshManager meshManager() throws NXException, RemoteException
NXException
RemoteException
FENodeLabelMap fenodeLabelMap() throws NXException, RemoteException
CAE.FENode
Label to CAE.FENode
Map for this
Interface to the Finite Element Model. Note: When accessing this map for an assembly fem,
it is the responsibility of the user to make sure that there are no node label conflicts.
If conflicts exist, there is no guarantee which node will be returned.
CAE.FENode
Label to CAE.FENode
MapNXException
RemoteException
FEElementLabelMap feelementLabelMap() throws NXException, RemoteException
CAE.FEElement
Label to CAE.FEElement
Map
for this Interface to the Finite Element Model. Note: When accessing this map for an assembly fem,
it is the responsibility of the user to make sure that there are no element label conflicts.
If conflicts exist, there is no guarantee which element will be returned.
CAE.FEElement
Label to CAE.FEElement
MapNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.