public interface FEElementLabelMap extends TransientObject
CAE.FEElement
map, it can be used to quickly convert
a CAE.FEElement
label, which is generally used in solver input files and results
files, in the element object itself CAE.FEElement
Modifier and Type | Method and Description |
---|---|
boolean |
askElementLabelUsed(int elementlabel)
Indicates whether input element label is already used or not
License requirements: nx_masterfem ("Finite Element Modeling") . |
int |
askNextElementLabel(int elementlabel)
Returns the next
CAE.FEElement label from the input put label. |
FEElement |
getElement(int elementlabel)
Returns
CAE.FEElement given a CAE.FEElement label
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX6.0.2 |
int |
numElements()
Returns the number of
CAE.FEElement
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX6.0.2 |
_value, dispose, printTestData, printTestData
FEElement getElement(int elementlabel) throws NXException, RemoteException
CAE.FEElement
given a CAE.FEElement
label
elementlabel
- CAE.FEElement
LabelCAE.FEElement
NXException
RemoteException
int numElements() throws NXException, RemoteException
CAE.FEElement
CAE.FEElement
NXException
RemoteException
int askNextElementLabel(int elementlabel) throws NXException, RemoteException
CAE.FEElement
label from the input put label.
elementlabel
- CAE.FEElement
Label, for first element label input 0CAE.FEElement
LabelNXException
RemoteException
boolean askElementLabelUsed(int elementlabel) throws NXException, RemoteException
elementlabel
- potential element labelNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.