public interface FEModelOccurrence extends IFEModel, IHierarchicalFEModel
Modifier and Type | Interface and Description |
---|---|
static class |
FEModelOccurrence.LabelOffsetsData
This class holds the data returned from
getLabelOffsets() |
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
TaggedObject |
find(String journalIdentifier)
Finds the object within the
FEModelOccurrence context,
with the given identifier as recorded in a journal. |
FEModelOccAttribute |
getAttributes()
Get the femodel occurrence attributes
License requirements: nx_masterfem ("Finite Element Modeling") . |
Component |
getComponent()
Gets the
Component associated with this
object
License requirements: None. |
FEModelOccurrence.LabelOffsetsData |
getLabelOffsets()
Returns node, element, and csys offset of the femodel occurrence
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
setLabelOffsets(int nodeOffset,
int elemOffset,
int csysOffset)
Sets node, element, and csys offset of the femodel occurrence
License requirements: nx_masterfem ("Finite Element Modeling") . |
feelementLabelMap, fenodeLabelMap, meshManager
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
getChildren, parent
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
FEModelOccurrence
context,
with the given identifier as recorded in a journal.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Journal identifier of the objectNXException
RemoteException
Component getComponent() throws NXException, RemoteException
NXException
RemoteException
FEModelOccurrence.LabelOffsetsData getLabelOffsets() throws NXException, RemoteException
NXException
RemoteException
void setLabelOffsets(int nodeOffset, int elemOffset, int csysOffset) throws NXException, RemoteException
nodeOffset
- node offsetelemOffset
- element offsetcsysOffset
- csys offsetNXException
RemoteException
FEModelOccAttribute getAttributes() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.