public interface FEModel extends BaseFEModel
CAE.FENode
) and Elements (CAE.FEElement
) in the model.
Only one instance of this class will exist in each fem part file
Modifier and Type | Interface and Description |
---|---|
static class |
FEModel.IdSpecificationObject
Structure to specify the Node, Element, and Physical property table start ids and offsets for use in
CAE.FEModel#appendFemodel |
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
AbstractionManager |
abstractionMgr()
Returns the circular imprint collection belonging to this fem part .
|
void |
appendFemodel(FEModel sourceFem,
FEModel.IdSpecificationObject idSpec)
This method appends finite element model data from a source fem
License requirements: nx_masterfem ("Finite Element Modeling") . |
TaggedObject |
find(String journalIdentifier)
Finds the
NXObject with the given identifier as recorded in a journal. |
LaminateGlobalLayupMgr |
globalLayupMgr()
Returns the laminate global layup manager belonging to the FEM.
|
beamSections, bolts, caeConnections, caeReuseLibrary, cfdAutoRefinementConstraints, cfdContactPreventionConstraints, cfdLocalResolutionConstraints, connectionElementCollection, connectionsRootFolder, enableFemUpdate, fluidDomains, meshControls, nodeElementMgr, updateFemodel
feelementLabelMap, fenodeLabelMap, meshManager
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
LaminateGlobalLayupMgr globalLayupMgr() throws RemoteException
RemoteException
AbstractionManager abstractionMgr() throws RemoteException
RemoteException
TaggedObject find(String journalIdentifier) throws NXException, RemoteException
NXObject
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Journal identifier of the objectNXException
RemoteException
void appendFemodel(FEModel sourceFem, FEModel.IdSpecificationObject idSpec) throws NXException, RemoteException
sourceFem
- Source finite element model to append data fromidSpec
- Node, Element, and Physical property table id specification objectNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.