NXOpen.UF.Disp.SystemParams Structure¶
NXOpen.UF.Disp.SystemParams is an alias for NXOpen.UF.DispSystemParams_Struct
-
class
NXOpen.UF.
DispSystemParams_Struct
¶ Bases:
object
Refer to UF_DISP_system_params_s for documentation.
Fields
NXOpen.UF.DispSystemParams_Struct.Tolerance |
Curve and surface tolerance |
NXOpen.UF.DispSystemParams_Struct.DashSize |
Dash size if font = 1 |
NXOpen.UF.DispSystemParams_Struct.SpaceSize |
Space size if font = 1 |
NXOpen.UF.DispSystemParams_Struct.SymbolSize |
symbol size in line font |
NXOpen.UF.DispSystemParams_Struct.FacetEdgeTol |
This is the facet edge tolerance for shaded display. |
NXOpen.UF.DispSystemParams_Struct.FacetChordTol |
This is the facet chord distance for shaded display. |
NXOpen.UF.DispSystemParams_Struct.FacetAngleTol |
This is the facet angle tolerance for shaded display. |
NXOpen.UF.DispSystemParams_Struct.Color |
system display color |
NXOpen.UF.DispSystemParams_Struct.PreselectionColor |
Preselection color. |
NXOpen.UF.DispSystemParams_Struct.HandleColor |
Handle color |
NXOpen.UF.DispSystemParams_Struct.Font |
system font mode1 = software line fonts 2 = hardware line fonts |
NXOpen.UF.DispSystemParams_Struct.ViewDisplay |
view names and borders display 1 = ON, 2 = OFF |
NXOpen.UF.DispSystemParams_Struct.LineWidthDisplay |
line width display mode 1 = yes, 2 = no |
NXOpen.UF.DispSystemParams_Struct.ShowShadedFaceEdges |
Specifies whether or not edges are displayed for shaded and analysis faces of solid and sheet bodies. |
NXOpen.UF.DispSystemParams_Struct.UseFaceEdgesColor |
Significant only if the show_shaded_- face_edges field is TRUE. |
NXOpen.UF.DispSystemParams_Struct.FaceEdgesColor |
Significant only if both the show_- shaded_face_edges field and the use_face_edges_color field are TRUE. |
NXOpen.UF.DispSystemParams_Struct.HiddenShadedFaceEdges |
Controls the appearance of hidden edges for shaded and analysis faces of solid and sheet bodies. |
NXOpen.UF.DispSystemParams_Struct.HiddenGeometryColor |
Significant only if the hidden_- shaded_face_edges field is not set to a color index. |
NXOpen.UF.DispSystemParams_Struct.RandomColorDisplayed |
Are random colors displayed for the part? If TRUE, random colors are displayed on the random color object type in the displayed part. |
NXOpen.UF.DispSystemParams_Struct.RandomColorObjectType |
Set to the type of objects on which random colors will be displayed. |