NXOpen.UF.DispSystemParams_Struct.FacetChordTol¶
-
DispSystemParams_Struct.
FacetChordTol
¶ This is the facet chord distance for shaded display. This is an upper bound on the distance from a positions on a facet to the surface. The recommended value is .005. A smaller value results in a finer display but causes degrade d performance. A value of .01 would give a coarse display, .0025 would give a fine display, .001 an extra fine display and .0005 an ultra fine display. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@