NXOpen.UF.DispSystemParams_Struct.HiddenShadedFaceEdges¶
-
DispSystemParams_Struct.
HiddenShadedFaceEdges
¶ Controls the appearance of hidden edges for shaded and analysis faces of solid and sheet bodies. If set to UF_DISP_INVISIBLE_HIDDEN_FACE_EDGES, hidden shaded face edges are not displayed. If set to UF_DISP_DASHED_- HIDDEN_FACE_EDGES, hidden shaded face edges are displayed like visible shaded face edges but with dashed line font. If set to a non-negative color index, hidden shaded face edges are displayed in this color, and the color is also used to display other hidden geometry where the geometry shows through shaded or analysis geometry.