NXOpen.UF.DispSystemParams_Struct.FacetEdgeTol¶
-
DispSystemParams_Struct.
FacetEdgeTol
¶ This is the facet edge tolerance for shaded display. This is an upper bound on the distance from each chord to the curve it is approximating The recommend value is .005. Smaller values result in finer display but causes degraded performance. A value of .01 would give a coarse display, .0005 would give an extra fine display. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@