AssignProxyBuilder Class |
Represents a NXOpen.Routing.Electrical.AssignProxyBuilder . |
CableConnection Class |
Connection used by a NXOpen.Routing.Electrical.CableDevice . |
CableConnectionCollection Class |
Represents a collection of NXOpen.Routing.Electrical.CableConnection objects. |
CableDefinition Class |
Holds the collection of wires in a NXOpen.Routing.Electrical.CableDevice . |
CableDevice Class |
Corresponds to a cable instance of an NXOpen.Routing.Electrical.ElectricalStockDevice . |
CableStockDefinition Class |
Describes a cable’s stock. |
CablewaysBuilder Class |
Represents NXOpen.Routing.Electrical.CablewaysBuilder . |
CablewaysLayoutBuilder Class |
Represents NXOpen.Routing.Electrical.CablewaysLayoutBuilder . |
CablewaysLayoutView Class |
Represents the CablewaysLayoutView class. |
CablewaysLayoutViewCollection Class |
Represents a collection of NXOpen.Routing.Electrical.CablewaysLayoutView objects. |
Connection Class |
|
ConnectionCollection Class |
Represents a collection of NXOpen.Routing.Electrical.Connection objects. |
ConnectorDevice Class |
The Electrical ConnectorDevice corresponds to a connector instance of NXOpen.Routing.SingleDevice . |
ConnectorDeviceCollection Class |
Represents a collection of NXOpen.Routing.Electrical.ConnectorDevice (CD) objects. |
ElectricalDeviceRelationship Class |
Represents a relationship between Routing Electrical devices.
|
ElectricalDeviceRelationshipCollection Class |
|
ElectricalFormat Class |
Represents a Routing Electrical ElectricalFormat. |
ElectricalFormatCollection Class |
Represents a Routing NXOpen.Routing.Electrical.ElectricalFormatCollection object. |
ElectricalNavigatorFilter Class |
Represents a Routing Electrical Navigator Filter object. |
ElectricalNavigatorFilterCollection Class |
Represents a Routing NXOpen.Routing.Electrical.ElectricalNavigatorFilterCollection object. |
ElectricalPartDefinitionShadow Class |
Represents NXOpen.Routing.Electrical.ElectricalPartDefinitionShadow object |
ElectricalStockDefinition Class |
Represents NXOpen.Routing.Electrical.ElectricalStockDefinition object |
ElectricalStockDevice Class |
The Electrical Stock Device is a non instantiable superclass to classify all electrical stock-based single devices. |
ElectricalStockDeviceCollection Class |
Represents a collection of NXOpen.Routing.Electrical.ElectricalStockDevice (ESD) objects. |
HarnessDefinition Class |
Represents a NXOpen.Routing.Electrical.HarnessDefinition |
HarnessDevice Class |
The Electrical HarnessDevice corresponds to a harness instance of the Routing.SingleDevice . |
HarnessDeviceCollection Class |
Represents a collection of Routing.Electrical.HarnessDevice objects. |
JumperConnection Class |
A jumper connection connects ports on the same connector.
|
JumperConnectionCollection Class |
A collection of NXOpen.Routing.Electrical.JumperConnection objects. |
NonPathConnection Class |
Describes a connection that does not have a path
|
NonPathConnectionCollection Class |
|
PathConnection Class |
Describes a connection that has a path
|
PathConnectionCollection Class |
|
ShieldDefinition Class |
Represents Routing Electrical ShieldDefinition object |
ShieldDevice Class |
The Electrical ShieldDevice corresponds to a shield instance of Routing.Electrical.ElectricalStockDevice . |
ShieldStockDefinition Class |
Represents Routing Electrical ShieldStockDefinition object |
SystemDefinition Class |
Represents a NXOpen.Routing.Electrical.SystemDefinition |
SystemDevice Class |
The Electrical SystemDevice corresponds to a system instance of the NXOpen.Routing.SingleDevice . |
SystemDeviceCollection Class |
Represents a collection of NXOpen.Routing.Electrical.SystemDevice objects. |
WireDevice Class |
The Electrical WireDevice corresponds to a wire instance of NXOpen.Routing.Electrical.ElectricalStockDevice . |