ElectricalFormat Class¶
-
class
NXOpen.Routing.Electrical.
ElectricalFormat
¶ Bases:
NXOpen.TaggedObject
Represents a Routing Electrical ElectricalFormat.
To create an instance of this class use
NXOpen.Routing.Electrical.ElectricalFormatCollection
New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
FormatType | Returns or sets the type of NXOpen.Routing.Electrical.ElectricalFormat |
Name | Returns or sets the name of NXOpen.Routing.Electrical.ElectricalFormat |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
ElectricalFormatType Enumeration | Describes how system reports the lengths of the stock. |
Property Detail¶
FormatType¶
-
ElectricalFormat.
FormatType
¶ Returns or sets the type of
NXOpen.Routing.Electrical.ElectricalFormat
-------------------------------------
Getter Method
Signature
FormatType()
Returns: Return type: NXOpen.Routing.Electrical.ElectricalFormatType
New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FormatType(type)
Parameters: type ( NXOpen.Routing.Electrical.ElectricalFormatType
) –New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Name¶
-
ElectricalFormat.
Name
¶ Returns or sets the name of
NXOpen.Routing.Electrical.ElectricalFormat
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX5.0.1.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)