Connection Class¶
-
class
NXOpen.Routing.Electrical.
Connection
¶ Bases:
NXOpen.Routing.LogicalConnection
The electrical usage of a
NXOpen.Routing.LogicalConnection
, restricted to one From and one To terminal.See NX Open Routing help for detailed information on the Connection data model.
Creator not available in KF.
New in version NX4.0.2.
Properties¶
Property | Description |
---|---|
FromTerminal | Returns or sets the From terminal. |
Guid | Returns or sets the object’s Global Unique Identifier (GUID). |
ImplementedBy | Returns the NXOpen.Routing.RouteObject implementing a connection. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaximumPathLength | Returns or sets the maximum path length for this connection. |
MinimumPathLength | Returns or sets the minimum path length for this connection. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PathLengthMultiplier | Returns or sets the path length multiplier. |
PathLengthOffset | Returns or sets the path length offset. |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
ToTerminal | Returns or sets the To terminal. |
Methods¶
Method | Description |
---|---|
AddFromTerminal | Add Routing.LogicalTerminal to the From Terminals collection. |
AddIntermediateTerminal | Add an intermediate terminal to this connection @return Was the NXOpen.Routing.LogicalTerminal added successfully? |
AddToTerminal | Add Routing.LogicalTerminal to end of the To Terminals collection. |
AssignPath | Assigns the given path to this connection and routes the connection on the path using the given routing level. |
AutomaticallyRoute | Automatically routes this connection on the shortest path using the given routing level. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindFromConnector | Get the From Connector for this connection. |
FindNearestCableDevice | Query this connection to find the nearest harness. |
FindNearestHarnessDevice | Query this connection to find the nearest harness. |
FindNearestParentDevice | Queries this connection for the nearest parent device. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
FindPaths | Returns all the possible paths this connection can use. |
FindToConnector | Get the To Connector for this connection. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetFromTerminals | Get all From Terminals from the logical connection @return Collection of Routing.LogicalTerminal |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIntermediateTerminals | Get the intermediate terminals associated with this connection. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetRoutedLevel | Gets the level used to route this connection. |
GetRoutedLevelEnum | Similar to NXOpen.Routing.Electrical.Connection.GetRoutedLevel() , but returns the NXOpen.Routing.Electrical.ConnectionRouteLevel enumeration instead of a string. |
GetRoutingMethod | Gets the method used to route this connection. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetToTerminals | Get all To Terminals from the logical connection @return Collection of Routing.LogicalTerminal |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
IsRouted | Is this connection routed? @return Is this connection routed? |
Prints a representation of this object to the system log file. | |
RemoveFromTerminal | Remove a Routing.LogicalTerminal from the From Terminals collection. |
RemoveIntermediateTerminal | Remove an intermediate terminal from this connection @return Was the NXOpen.Routing.LogicalTerminal removed successfully? |
RemoveToTerminal | Remove a Routing.LogicalTerminal from the To Terminals collection. |
ReplaceFromTerminals | Replace the existing From Terminals for the logical connection with collection of Routing.LogicalTerminal terminals |
ReplaceIntermediateTerminals | Replaces the intermediate terminals associated with this connection. |
ReplaceToTerminals | Replace the existing To Terminals for the logical connection with collection of Routing.LogicalTerminal terminals |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristic2 | Sets or creates an integer type attribute associated with the input title. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetCharacteristics2 | Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unroute | Unroutes this connection. |
Enumerations¶
ConnectionRouteLevel Enumeration | Routing level. |
Property Detail¶
FromTerminal¶
-
Connection.
FromTerminal
¶ Returns or sets the From terminal.
The From terminal is one end of an electrical connection. From does not imply an ordering.
-------------------------------------
Getter Method
Signature
FromTerminal()
Returns: Return type: NXOpen.Routing.LogicalTerminal
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FromTerminal(fromTerminal)
Parameters: fromTerminal ( NXOpen.Routing.LogicalTerminal
) – May not be NoneNew in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
IsOccurrence¶
-
Connection.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Connection.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaximumPathLength¶
-
Connection.
MaximumPathLength
¶ Returns or sets the maximum path length for this connection.
Maximum path length is the longest allowable length of all segments referred to by this connection.
-------------------------------------
Getter Method
Signature
MaximumPathLength()
Returns: May be zero Return type: float New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
MaximumPathLength(pathLength)
Parameters: pathLength (float) – May be zero New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
MinimumPathLength¶
-
Connection.
MinimumPathLength
¶ Returns or sets the minimum path length for this connection.
Minimum path length is the shortest allowable length of all segments referred to by this connection.
-------------------------------------
Getter Method
Signature
MinimumPathLength()
Returns: May be zero Return type: float New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
MinimumPathLength(pathLength)
Parameters: pathLength (float) – May be zero New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Name¶
-
Connection.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Connection.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Connection.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PathLengthMultiplier¶
-
Connection.
PathLengthMultiplier
¶ Returns or sets the path length multiplier.
Used to calculate cut length. Cut length = length * multiplier + offset
-------------------------------------
Getter Method
Signature
PathLengthMultiplier()
Returns: May be zero (cut length will be zero) Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
PathLengthMultiplier(pathLengthMultiplier)
Parameters: pathLengthMultiplier (str) – May be zero (cut length will be zero) New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
PathLengthOffset¶
-
Connection.
PathLengthOffset
¶ Returns or sets the path length offset.
Used to calculate cut length. Cut length = length * multiplier + offset
-------------------------------------
Getter Method
Signature
PathLengthOffset()
Returns: May be zero Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
PathLengthOffset(pathLengthOffset)
Parameters: pathLengthOffset (str) – May be zero New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Prototype¶
-
Connection.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ToTerminal¶
-
Connection.
ToTerminal
¶ Returns or sets the To terminal.
The To terminal is one end of an electrical connection. To does not imply an ordering
-------------------------------------
Getter Method
Signature
ToTerminal()
Returns: Return type: NXOpen.Routing.LogicalTerminal
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ToTerminal(toTerminal)
Parameters: toTerminal ( NXOpen.Routing.LogicalTerminal
) – May not be NoneNew in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
AddIntermediateTerminal¶
-
Connection.
AddIntermediateTerminal
¶ Add an intermediate terminal to this connection
Signature
AddIntermediateTerminal(intermediateTerminal)
Parameters: intermediateTerminal ( NXOpen.Routing.LogicalTerminal
) – Can not be NoneReturns: Was the NXOpen.Routing.LogicalTerminal
added successfully?Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
AssignPath¶
-
Connection.
AssignPath
¶ Assigns the given path to this connection and routes the connection on the path using the given routing level.
Use
NXOpen.Routing.Electrical.Connection.FindPaths()
to find all available paths for this connection.Signature
AssignPath(routeLevel, path)
Parameters: - routeLevel (
NXOpen.Routing.Electrical.ConnectionRouteLevel
) – - path (
NXOpen.Routing.Path
) – The path on which to route this connection.
New in version NX8.0.3.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
- routeLevel (
AutomaticallyRoute¶
-
Connection.
AutomaticallyRoute
¶ Automatically routes this connection on the shortest path using the given routing level.
Signature
AutomaticallyRoute(routeLevel)
Parameters: routeLevel ( NXOpen.Routing.Electrical.ConnectionRouteLevel
) –New in version NX8.0.3.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
DeleteCharacterstics¶
-
Connection.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindFromConnector¶
-
Connection.
FindFromConnector
¶ Get the From Connector for this connection.
From does not imply an ordering.
Signature
FindFromConnector()
Returns: May be None Return type: NXOpen.Routing.Electrical.ConnectorDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindNearestCableDevice¶
-
Connection.
FindNearestCableDevice
¶ Query this connection to find the nearest harness.
Only finds a cable that is a parent to this connection at some level up the connection heirarchy.
Signature
FindNearestCableDevice()
Returns: Will be None if connection is not in a cable Return type: NXOpen.Routing.Electrical.CableDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindNearestHarnessDevice¶
-
Connection.
FindNearestHarnessDevice
¶ Query this connection to find the nearest harness.
Only finds a harness that is a parent to this connection at some level up the connection heirarchy.
Signature
FindNearestHarnessDevice()
Returns: May be None if connection is not in a harness Return type: NXOpen.Routing.Electrical.HarnessDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindNearestParentDevice¶
-
Connection.
FindNearestParentDevice
¶ Queries this connection for the nearest parent device.
The nearest parent device is either a cable, shield, or harness
Signature
FindNearestParentDevice()
Returns: Will be None if connection is not in a harness, cable, or shield. Return type: NXOpen.Routing.SingleDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindObject¶
-
Connection.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
FindPaths¶
-
Connection.
FindPaths
¶ Returns all the possible paths this connection can use.
Signature
FindPaths(routeLevel)
Parameters: routeLevel ( NXOpen.Routing.Electrical.ConnectionRouteLevel
) –Returns: Possible paths this connection can use. Return type: list of NXOpen.Routing.Path
New in version NX8.0.3.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FindToConnector¶
-
Connection.
FindToConnector
¶ Get the To Connector for this connection.
To does not imply an ordering
Signature
FindToConnector()
Returns: May be None Return type: NXOpen.Routing.Electrical.ConnectorDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetCharacteristics¶
-
Connection.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
Connection.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
Connection.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntermediateTerminals¶
-
Connection.
GetIntermediateTerminals
¶ Get the intermediate terminals associated with this connection.
Intermediate Terminals are optional and need not exist for a
NXOpen.Routing.Electrical.Connection
to be valid in NX.Signature
GetIntermediateTerminals()
Returns: Collection of intermediate NXOpen.Routing.LogicalTerminal
- May be NoneReturn type: list of NXOpen.Routing.LogicalTerminal
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
Connection.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRoutedLevel¶
-
Connection.
GetRoutedLevel
¶ Gets the level used to route this connection.
Signature
GetRoutedLevel()
Returns: - “C” Connection routed at component level
- “P” Connection routed at pin level
- “M” Connection routed at mixed level
Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRoutedLevelEnum¶
-
Connection.
GetRoutedLevelEnum
¶ Similar to
NXOpen.Routing.Electrical.Connection.GetRoutedLevel()
, but returns theNXOpen.Routing.Electrical.ConnectionRouteLevel
enumeration instead of a string.Signature
GetRoutedLevelEnum()
Returns: Route level. Return type: NXOpen.Routing.Electrical.ConnectionRouteLevel
New in version NX8.0.3.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetRoutingMethod¶
-
Connection.
GetRoutingMethod
¶ Gets the method used to route this connection.
Signature
GetRoutingMethod()
Returns: - “A” Connection is auto routed
- “M” Connection is manual routed
- “N” Connection is not routed
Return type: str New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
Connection.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
IsRouted¶
-
Connection.
IsRouted
¶ Is this connection routed?
Signature
IsRouted()
Returns: Is this connection routed? Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Print¶
-
Connection.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveIntermediateTerminal¶
-
Connection.
RemoveIntermediateTerminal
¶ Remove an intermediate terminal from this connection
Signature
RemoveIntermediateTerminal(intermediateTerminal)
Parameters: intermediateTerminal ( NXOpen.Routing.LogicalTerminal
) – may be NoneReturns: Was the NXOpen.Routing.LogicalTerminal
removed successfully?Return type: bool New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ReplaceIntermediateTerminals¶
-
Connection.
ReplaceIntermediateTerminals
¶ Replaces the intermediate terminals associated with this connection.
Signature
ReplaceIntermediateTerminals(intermediateTerminals)
Parameters: intermediateTerminals (list of NXOpen.Routing.LogicalTerminal
) – Collection of intermediateNXOpen.Routing.LogicalTerminal
- Use None to remove all intermdiate terminalsNew in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetCharacteristic¶
-
Connection.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (int) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (float) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (str) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristic2¶
-
Connection.
SetCharacteristic2
¶ Overloaded method SetCharacteristic2
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
-------------------------------------
Sets or creates an integer type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (int) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a double type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (float) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a string type type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (str) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
Connection.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristics2()
instead.License requirements: routing_base (“Routing Basic”)
SetCharacteristics2¶
-
Connection.
SetCharacteristics2
¶ Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit part attributes on the stock part. For legacy parts where the attributes are on the stock component, the attributes will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit attributes on the corresponding instance. For legacy parts where the attribute is on the component, the attributes will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create attributes on the object itself.
Signature
SetCharacteristics2(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –NXOpen.Routing.CharacteristicList
having the titles, types and values of Attributes to be setNew in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
Connection.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.