ConnectionRouteLevel Enumeration¶
NXOpen.Routing.Electrical.Connection.RouteLevel is an alias for NXOpen.Routing.Electrical.ConnectionRouteLevel
-
class
NXOpen.Routing.Electrical.
ConnectionRouteLevel
¶ Bases:
object
Routing level.
Enum Members
Enum Member Enum Member Description NotRouted Pin Route to the pin on the connector component.Component Route to the connector component directly without regard for the pins.Mixed Route to the pin, if possible, otherwise route to the component.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-