CableDefinition Class¶
-
class
NXOpen.Routing.Electrical.
CableDefinition
¶ Bases:
NXOpen.Routing.AssemblyDefinition
Holds the collection of wires in a
NXOpen.Routing.Electrical.CableDevice
.A cable consists of both a
NXOpen.Routing.Electrical.CableDevice
and aNXOpen.Routing.Electrical.CableDefinition
. ANXOpen.Routing.Electrical.CableDevice
object uses aNXOpen.Routing.Electrical.CableDefinition
to hold a collection ofNXOpen.Routing.Electrical.WireDevice
objects and/orNXOpen.Routing.Electrical.CableDevice
objects contained by the cable. This definition corresponds to AP212 Assembly_definition.See the NX Routing help for detailed information on the Connection data model.
Creator not available in KF.
New in version NX4.0.2.
Properties¶
Property | Description |
---|---|
DefiningNxObject | Returns the NX object associated with the item definition object. |
Guid | Returns or sets the object’s Global Unique Identifier (GUID). |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddSingleDeviceChild | Adds a NXOpen.Routing.SingleDevice object to the list of objects contained in the assembly. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteCharacterstics | Removes the input list of characteristics from this object. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCharacteristics | Get all of the characteristics values on the this object. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDestinationCharacteristics | Returns the destination characteristics from the input object. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerCharacteristic | Get the value of an integer characteristic associated with the input name. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealCharacteristic | Get the value of a real characteristic associated with the input name. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetReferencingDevice | Gets the NXOpen.Routing.SingleDevice object that has this AssemblyDefinition object as its definition. |
GetSingleDeviceChildren | Gets the list of NXOpen.Routing.SingleDevice objects contained in the assembly. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringCharacteristic | Get the value of a string characteristic associated with the input name. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
IsSingleDeviceChild | Determines if a NXOpen.Routing.SingleDevice object is contained in the assembly @return TRUE if the object is in the AssemblyDefinition |
Prints a representation of this object to the system log file. | |
RemoveSingleDeviceChild | Removes a NXOpen.Routing.SingleDevice from the list of objects contained in the assembly. |
ReplaceSingleDeviceChildren | Replaces the list of NXOpen.Routing.SingleDevice objects contained in the assembly. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetCharacteristic | Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. |
SetCharacteristic2 | Sets or creates an integer type attribute associated with the input title. |
SetCharacteristics | Set all of the characteristics values on this object. |
SetCharacteristics2 | Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
CableDefinition.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CableDefinition.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CableDefinition.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CableDefinition.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CableDefinition.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CableDefinition.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
DeleteCharacterstics¶
-
CableDefinition.
DeleteCharacterstics
¶ Removes the input list of characteristics from this object.
Signature
DeleteCharacterstics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FindObject¶
-
CableDefinition.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCharacteristics¶
-
CableDefinition.
GetCharacteristics
¶ Get all of the characteristics values on the this object.
Signature
GetCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetDestinationCharacteristics¶
-
CableDefinition.
GetDestinationCharacteristics
¶ Returns the destination characteristics from the input object.
Retrieves the description of which destination characteristics to read from the application view and then reads those destination characteristics from the object
- Ports: Reads characteristics from the port.
- RCPs: Attempts to find a port at the RCP, reads characteristics from
the port if it exists, otherwise reads from the stock associated with the rcp.
- Segments: Reads characteristics from the stock associated with the segment.
- Components: Reads characteristics directly from the component.
- Stock: Reads characteristics from the stock or from the stock’s data.
Signature
GetDestinationCharacteristics()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetIntegerCharacteristic¶
-
CableDefinition.
GetIntegerCharacteristic
¶ Get the value of an integer characteristic associated with the input name.
Signature
GetIntegerCharacteristic(name)
Parameters: name (str) – Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRealCharacteristic¶
-
CableDefinition.
GetRealCharacteristic
¶ Get the value of a real characteristic associated with the input name.
Signature
GetRealCharacteristic(name)
Parameters: name (str) – Returns: Return type: float New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetStringCharacteristic¶
-
CableDefinition.
GetStringCharacteristic
¶ Get the value of a string characteristic associated with the input name.
Signature
GetStringCharacteristic(name)
Parameters: name (str) – Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Print¶
-
CableDefinition.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetCharacteristic¶
-
CableDefinition.
SetCharacteristic
¶ Overloaded method SetCharacteristic
SetCharacteristic(name, value)
SetCharacteristic(name, value)
SetCharacteristic(name, value)
-------------------------------------
Set the value of an integer characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to integer if it’s type is not integer.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (int) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an real characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to real if it’s type is not real.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (float) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
Set the value of an string characteristic associated with the input name, adds a new characteristic to the list if one doesn’t exist already. Converts the type of an existing characteristic with the same name to string if it’s type is not string.
Signature
SetCharacteristic(name, value)
Parameters: - name (str) –
- value (str) –
New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristic2()
instead.License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristic2¶
-
CableDefinition.
SetCharacteristic2
¶ Overloaded method SetCharacteristic2
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
SetCharacteristic2(title, value)
-------------------------------------
Sets or creates an integer type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (int) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a double type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (float) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Sets or creates a string type type attribute associated with the input title. creating a new attribute if one doesn’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit a part attribute on the stock part. For legacy parts where the attribute is on the stock component, the attribute will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit an attribute on the corresponding instance. For legacy parts where the attribute is on the component, the attribute will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create an attribute on the object itself.
Signature
SetCharacteristic2(title, value)
Parameters: - title (str) – Unique title for the Attribute or Characteristic
- value (str) – New Value to be set on the Attribute
New in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
SetCharacteristics¶
-
CableDefinition.
SetCharacteristics
¶ Set all of the characteristics values on this object.
Signature
SetCharacteristics(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –New in version NX4.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Routing.ICharacteristic.SetCharacteristics2()
instead.License requirements: routing_base (“Routing Basic”)
SetCharacteristics2¶
-
CableDefinition.
SetCharacteristics2
¶ Sets all attributes associated with the titles from the input list, creating new attributes for the ones that don’t exist already.
If the method is called on a stock
Assemblies.Component
, the method will create or edit part attributes on the stock part. For legacy parts where the attributes are on the stock component, the attributes will be moved to the stock part.If the method is called on a non-stock
Assemblies.Component
, the method will create or edit attributes on the corresponding instance. For legacy parts where the attribute is on the component, the attributes will be moved to the corresponding instance.If the method is called on any non-component object, the method will access or create attributes on the object itself.
Signature
SetCharacteristics2(values)
Parameters: values ( NXOpen.Routing.CharacteristicList
) –NXOpen.Routing.CharacteristicList
having the titles, types and values of Attributes to be setNew in version NX11.0.0.
License requirements: routing_base (“Routing Basic”)
SetName¶
-
CableDefinition.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.