RoutingPart Class¶
-
class
NXOpen.Preferences.
RoutingPart
¶ Bases:
object
Contains the preferences related to placing/finding/adding parts and generating the Routing bill of materials.
To obtain an instance of this class, refer to
NXOpen.Preferences.RoutingApplicationView
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BomDetailLevelFlag | Returns or sets the detail level for the Routing bill of material. |
BomFormatPart | Returns or sets the name of the template Routing bill of material part file. |
DefaultElbowNode | Returns or sets the node in the part library to use for searching for the default elbow to place during create path. |
FabricationNumberingFlag | Returns or sets the fabrication numbering for the Routing bill of material. |
InvalidSequenceCharacters | Returns or sets the list of characters that cannot be used when generating sequences of terminals in qualify part. |
Layer | Returns or sets the layer to apply to new components. |
MaximumSolutions | Returns or sets the maximum number of placement solutions to generate when determining placement solutions for a component. |
PreferredPortMethodFlag | Returns the current method for determining the preferred placement port. |
StockLengthDisplayFlag | Returns or sets the stock length display for the Routing bill of material. |
UsePreferredPortFlag | Returns or sets whether or not to use the preffered placement port during calcluation of placement solutions during place part. |
PartLibrary |
|
Methods¶
Method | Description |
---|---|
GetPreferredPortAttribute | Gets the attribute and it’s value for determining the preferred port for method type NXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute |
GetPreferredPortName | Gets the desired port name for method type NXOpen.Preferences.RoutingPartPreferredPortMethod.Name @return None if method is not NXOpen.Preferences.RoutingPartPreferredPortMethod.Name |
SetPreferredPortAttribute | Sets the method for determining the preferred port to NXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute and sets the desired port attribute and it’s value. |
SetPreferredPortName | Sets the method for determining the preferred port to NXOpen.Preferences.RoutingPartPreferredPortMethod.Name and sets the desired port name. |
Enumerations¶
RoutingPartDetailLevel Enumeration | The detail levels available for the Routing bill of material. |
RoutingPartFabricationNumbering Enumeration | The fabrication numbering methods available for the Routing bill of material. |
RoutingPartPreferredPortMethod Enumeration | Available methods for determining which port is the preferredport during calculation of placement solutions. |
RoutingPartStockLengthDisplay Enumeration | The stock length display options available for the Routing bill of material. |
RoutingPartUsePreferredPort Enumeration | Whether or not use the preferred port when determining placement solutions. |
Property Detail¶
BomDetailLevelFlag¶
-
RoutingPart.
BomDetailLevelFlag
¶ Returns or sets the detail level for the Routing bill of material.
-------------------------------------
Getter Method
Signature
BomDetailLevelFlag()
Returns: Return type: NXOpen.Preferences.RoutingPartDetailLevel
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BomDetailLevelFlag(detail)
Parameters: detail ( NXOpen.Preferences.RoutingPartDetailLevel
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
BomFormatPart¶
-
RoutingPart.
BomFormatPart
¶ Returns or sets the name of the template Routing bill of material part file.
-------------------------------------
Getter Method
Signature
BomFormatPart()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BomFormatPart(bomPart)
Parameters: bomPart (str) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
DefaultElbowNode¶
-
RoutingPart.
DefaultElbowNode
¶ Returns or sets the node in the part library to use for searching for the default elbow to place during create path.
The part library node must have a type of
NXOpen.Preferences.RoutingPartLibraryNodeType.Table
. A None node indicates no default elbow part table.-------------------------------------
Getter Method
Signature
DefaultElbowNode()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DefaultElbowNode(elbowNode)
Parameters: elbowNode (str) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FabricationNumberingFlag¶
-
RoutingPart.
FabricationNumberingFlag
¶ Returns or sets the fabrication numbering for the Routing bill of material.
-------------------------------------
Getter Method
Signature
FabricationNumberingFlag()
Returns: Return type: NXOpen.Preferences.RoutingPartFabricationNumbering
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FabricationNumberingFlag(numbering)
Parameters: numbering ( NXOpen.Preferences.RoutingPartFabricationNumbering
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
InvalidSequenceCharacters¶
-
RoutingPart.
InvalidSequenceCharacters
¶ Returns or sets the list of characters that cannot be used when generating sequences of terminals in qualify part.
-------------------------------------
Getter Method
Signature
InvalidSequenceCharacters()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
InvalidSequenceCharacters(invalidChars)
Parameters: invalidChars (str) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
Layer¶
-
RoutingPart.
Layer
¶ Returns or sets the layer to apply to new components.
-------------------------------------
Getter Method
Signature
Layer()
Returns: The layer to place the new component on -1 means use the original layers defined in the component. 0 means use the work layer. 1-256 means use the specified layer. :rtype: int
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
Layer(layer)
Parameters: layer (int) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
MaximumSolutions¶
-
RoutingPart.
MaximumSolutions
¶ Returns or sets the maximum number of placement solutions to generate when determining placement solutions for a component.
-------------------------------------
Getter Method
Signature
MaximumSolutions()
Returns: Return type: int New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
MaximumSolutions(maxSols)
Parameters: maxSols (int) – New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
PreferredPortMethodFlag¶
-
RoutingPart.
PreferredPortMethodFlag
¶ Returns the current method for determining the preferred placement port.
-------------------------------------
Getter Method
Signature
PreferredPortMethodFlag()
Returns: Return type: NXOpen.Preferences.RoutingPartPreferredPortMethod
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
StockLengthDisplayFlag¶
-
RoutingPart.
StockLengthDisplayFlag
¶ Returns or sets the stock length display for the Routing bill of material.
-------------------------------------
Getter Method
Signature
StockLengthDisplayFlag()
Returns: Return type: NXOpen.Preferences.RoutingPartStockLengthDisplay
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StockLengthDisplayFlag(display)
Parameters: display ( NXOpen.Preferences.RoutingPartStockLengthDisplay
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
UsePreferredPortFlag¶
-
RoutingPart.
UsePreferredPortFlag
¶ Returns or sets whether or not to use the preffered placement port during calcluation of placement solutions during place part.
-------------------------------------
Getter Method
Signature
UsePreferredPortFlag()
Returns: Return type: NXOpen.Preferences.RoutingPartUsePreferredPort
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
UsePreferredPortFlag(useFlag)
Parameters: useFlag ( NXOpen.Preferences.RoutingPartUsePreferredPort
) –New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
PartLibrary¶
-
RoutingPart.
PartLibrary
¶ The Routing part library.
Signature
PartLibrary()
New in version NX3.0.0.
Returns: Return type: NXOpen.Preferences.RoutingPartLibrary
Method Detail¶
GetPreferredPortAttribute¶
-
RoutingPart.
GetPreferredPortAttribute
¶ Gets the attribute and it’s value for determining the preferred port for method type
NXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute
Signature
GetPreferredPortAttribute()
Returns: a tuple Return type: A tuple consisting of (attributeName, attributeValue). attributeName is a str. None if method is not
NXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute
attributeValue is a str. None if method is notNXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute
.. versionadded:: NX4.0.0License requirements: routing_base (“Routing Basic”)
GetPreferredPortName¶
-
RoutingPart.
GetPreferredPortName
¶ Gets the desired port name for method type
NXOpen.Preferences.RoutingPartPreferredPortMethod.Name
Signature
GetPreferredPortName()
Returns: None if method is not NXOpen.Preferences.RoutingPartPreferredPortMethod.Name
:rtype: strNew in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetPreferredPortAttribute¶
-
RoutingPart.
SetPreferredPortAttribute
¶ Sets the method for determining the preferred port to
NXOpen.Preferences.RoutingPartPreferredPortMethod.Attribute
and sets the desired port attribute and it’s value.Signature
SetPreferredPortAttribute(attributeName, attributeValue)
Parameters: - attributeName (str) – Attribute name on port to match. Must not be None and the length of the string must be less than 50.
- attributeValue (str) – Value of the attribute to match.
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
SetPreferredPortName¶
-
RoutingPart.
SetPreferredPortName
¶ Sets the method for determining the preferred port to
NXOpen.Preferences.RoutingPartPreferredPortMethod.Name
and sets the desired port name.Signature
SetPreferredPortName(desiredPort)
Parameters: desiredPort (str) – Port name to match. Must not be None and the length of the string must be less than 50. New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)