RoutingPartLibrary Class¶
-
class
NXOpen.Preferences.
RoutingPartLibrary
¶ Bases:
object
Represents a Routing Part library.
To obtain an instance of this class, refer to
NXOpen.Preferences.RoutingPart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateCriteria | Creates a new empty NXOpen.Routing.CharacteristicList object that can be used as input to Preferences.RoutingPartLibrary.MatchCriteria() and Preferences.RoutingPartLibrary.MatchCriteriaWithFilter() . |
FilterOnCurrentSpecifications | Does a characteristic list match the current discipline and specifications? @return Is the characteristic list valid under the current discipline and specifications? |
GetChildrenNodes | Returns the children nodes of the input node. |
GetFilteredRoot | Returns the root node of the part library using the current active discipline. |
GetNodeType | Returns the node type. |
GetPartDefinition | Returns the part information for a given NXOpen.Preferences.RoutingPartLibraryNodeType.Part node. |
GetRoot | Returns the root node of the part library. |
GetTableDefinition | Returns the table information for a given NXOpen.Preferences.RoutingPartLibraryNodeType.Table node. |
MatchCriteria | Search for entries in the part library table nodes that match the given set of criteria. |
MatchCriteriaWithFilter | Similar to Preferences.RoutingPartLibrary.MatchCriteria() , however it also filters out any parts that don’t match the critiera specified by the current specification. |
Enumerations¶
RoutingPartLibraryColumnStatus Enumeration | Hidden status of a column. |
RoutingPartLibraryColumnType Enumeration | Type of column values. |
RoutingPartLibraryNodeType Enumeration | Type of nodes in the part library. |
RoutingPartLibraryRootType Enumeration | Type of root nodes. |
Structs¶
RoutingPartLibraryColumn_Struct Struct | Part table column type. |
Method Detail¶
CreateCriteria¶
-
RoutingPartLibrary.
CreateCriteria
¶ Creates a new empty
NXOpen.Routing.CharacteristicList
object that can be used as input toPreferences.RoutingPartLibrary.MatchCriteria()
andPreferences.RoutingPartLibrary.MatchCriteriaWithFilter()
.Signature
CreateCriteria()
Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
FilterOnCurrentSpecifications¶
-
RoutingPartLibrary.
FilterOnCurrentSpecifications
¶ Does a characteristic list match the current discipline and specifications?
Signature
FilterOnCurrentSpecifications(match, partClasses)
Parameters: - match (
NXOpen.Routing.CharacteristicList
) – The matching part’s Characteristic List to check against the current discipline and specifications. - partClasses (list of str) – The part class hierarchy list that contains the matching part. The first item in the list is the top node name. The last item in the list is the lowest node that contains the matching part.
Returns: Is the characteristic list valid under the current discipline and specifications?
Return type: bool
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- match (
GetChildrenNodes¶
-
RoutingPartLibrary.
GetChildrenNodes
¶ Returns the children nodes of the input node.
Signature
GetChildrenNodes(parent)
Parameters: parent (str) – Returns: Return type: list of str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetFilteredRoot¶
-
RoutingPartLibrary.
GetFilteredRoot
¶ Returns the root node of the part library using the current active discipline.
Returns None if there is no root node.
Signature
GetFilteredRoot(rootType)
Parameters: rootType ( NXOpen.Preferences.RoutingPartLibraryRootType
) – Which root node to find.Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetNodeType¶
-
RoutingPartLibrary.
GetNodeType
¶ Returns the node type.
Signature
GetNodeType(node)
Parameters: node (str) – Returns: Return type: NXOpen.Preferences.RoutingPartLibraryNodeType
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetPartDefinition¶
-
RoutingPartLibrary.
GetPartDefinition
¶ Returns the part information for a given
NXOpen.Preferences.RoutingPartLibraryNodeType.Part
node.Signature
GetPartDefinition(node)
Parameters: node (str) – Must be a NXOpen.Preferences.RoutingPartLibraryNodeType.Part
type node, any other node type causes an exception.Returns: Return type: NXOpen.Routing.CharacteristicList
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetRoot¶
-
RoutingPartLibrary.
GetRoot
¶ Returns the root node of the part library.
Returns None if there is no root node.
Signature
GetRoot()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
GetTableDefinition¶
-
RoutingPartLibrary.
GetTableDefinition
¶ Returns the table information for a given
NXOpen.Preferences.RoutingPartLibraryNodeType.Table
node.Signature
GetTableDefinition(node)
Parameters: node (str) – Must be a NXOpen.Preferences.RoutingPartLibraryNodeType.Table
type node, any other node type causes an exception.Returns: Return type: list of NXOpen.Preferences.RoutingPartLibraryColumn_Struct
New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
MatchCriteria¶
-
RoutingPartLibrary.
MatchCriteria
¶ Search for entries in the part library table nodes that match the given set of criteria.
Returns an array of
NXOpen.Routing.CharacteristicList
objects that can be used for assigning stock or placing parts. Searches all nodes at or below the input node for matches.Performs matches on the name/value pairs in the input critiera, to the column name column values in the part tables below the input node. Ignores names in the input critiera that don’t have a corresonding column in the part for matching.
Signature
MatchCriteria(startNode, criteria)
Parameters: - startNode (str) – Must not be a
NXOpen.Preferences.RoutingPartLibraryNodeType.Part
node. - criteria (
NXOpen.Routing.CharacteristicList
) –
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- startNode (str) – Must not be a
MatchCriteriaWithFilter¶
-
RoutingPartLibrary.
MatchCriteriaWithFilter
¶ Similar to
Preferences.RoutingPartLibrary.MatchCriteria()
, however it also filters out any parts that don’t match the critiera specified by the current specification.Signature
MatchCriteriaWithFilter(startNode, criteria)
Parameters: - startNode (str) – Must not be a
NXOpen.Preferences.RoutingPartLibraryNodeType.Part
node. - criteria (
NXOpen.Routing.CharacteristicList
) –
Returns: Return type: New in version NX4.0.0.
License requirements: routing_base (“Routing Basic”)
- startNode (str) – Must not be a