RoutingPartLibraryColumnType Enumeration

NXOpen.Preferences.RoutingPartLibrary.ColumnType is an alias for NXOpen.Preferences.RoutingPartLibraryColumnType

class NXOpen.Preferences.RoutingPartLibraryColumnType

Bases: object

Type of column values.

Enum Members

Enum Member Enum Member Description
Integer
Integer values.
Real
Floating-point values.
String
String values.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.